Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84791members
354240posts

M340 M580 X80 firmware file links V5.0

Alliance System Integrators Forum

A private forum for Schneider Electric’s Alliance System Integrators to share best practices, information, documents, event details, and business opportunities.

AlastairF
Lieutenant Lieutenant
Lieutenant
0 Likes
0
524

M340 M580 X80 firmware file links V5.0

M340/ M580/ X80 firmware file links V5.0

This is a more comprehensive package of links (Firmware link spreadsheet V5.0) than the one provided with SESU.

New update as at 2021-02-04

The attached spreadsheet lists collated links to publicly available firmware for M340/ M580/ X80/ Advantys/ Connexium.

Updated with:

  • all embedded links point to se.com public sources
  • X80 updates
  • MC80 added
  • New firmware for BMENUA and BMENOR modules.

 

Feedback welcome (broken links, improvements or additions needed).

The new EcoStruxure Automation Device Maintenance (EADM) tool is now available (link in the spreadsheet). At the moment there is no cloud connectivity for firmware updates so the spreadsheet is still a useful source. Follow the instructions in EADM Help to place the FW files into the correct location for EADM to use.

EADM is mandatory for BMENUA and BMENOR module FW upgrades.

Attachments
Tags (1)