Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84690members
354060posts

Headless Monitoring

Alliance System Integrators Forum

A private forum for Schneider Electric’s Alliance System Integrators to share best practices, information, documents, event details, and business opportunities.

Arinia
Crewman
Crewman
2
2355

Headless Monitoring

Hello, everyone. We've got two SmartUPS 2000 and two SmartUPS SRT 8000 devices in our IDF rooms on several floors of the office. Since there are no servers in the IDF rooms, only network equipment, I need to find a way to utilize the remote management features of the NMCs that we've installed or that came preinstalled on those units. My company won't spend the money for the Struxure Ware azarchat DCE software and the Power Chute Business Edition is only applicable for devices that are connected via serial cable to an actual server or PC with the Power Chute agent installed on it. I've looked everywhere I can think of and have not been able to find a solution, so I'm hoping someone out there may have a suggestion that would help? Thanks in advance for any assistance anyone can provide.

Thanks

Tags (1)
2 Replies 2
Paolo_Colombo
Lieutenant Lieutenant
Lieutenant
0 Likes
1
2351

Re: Headless Monitoring

Hi

Normally PowerChute is used to gracefully shutdown your servers/PCs, if you need to monitor the Smart UPS you can easily register and use the online EcoStruxure IT function to monitor

 

From this link you will find the instruction to connect

Smart-UPS™ - For Business (apc.com)

 

Best

Paolo

 

 

 

 

 

 

Industrial Channels go to market Director
Secure Power Division - Commercial & Industrial

Those who can imagine anything, can create the impossible. (Alan Turing)
Tags (1)
George856
Cadet
0 Likes
0
2210

Headless testing is simply running your Selenium tests using a headless browser. It operates as your typical browser would, butRe: Headless Monitoring

Headless testing is simply running your Selenium tests using a headless browser. It operates as your typical browser would, but without a user interface, making it excellent for automated testing.

 

 

RapidFS

Tags (1)