Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
A support forum for AVEVA Plant SCADA (formerly Citect SCADA). Share new and exciting product information, connect, learn, and collaborate with the ecosystem of Plant SCADA Users. AVEVA Plant SCADA a reliable, flexible and high-performance Supervisory Control and Data Acquisition software solution for industrial process customers. This forum is to connect, share, learn and collaborate new and exciting product information. Feel free to join and share to your Ecosystem of Plant SCADA Users.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-26 07:43 PM
There are two ways to communicate between M580 and AVRAV Plant SCADA over Modbus TCP/IP. What is the suggested/recommended protocol to use for an around 25K tags AVEVA Plant SCADA with M580 PLCs, MODNET or OFSOPC??
I notice there are some issues on OFS with the older versions not not sure any issue or limitation with the current version 3.62 now before my mass deployment. Thanks in advance for your comments and feedback.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-02-18 12:00 AM
Well.. In my view if you looking for cross platform and you are planning to move from old hardware to newer hardware versions of controller and devices (IOT compatible) with cybersecurity and its always advisable to use OPC UA/OPC UA Embedded (NUA) over OPC DA as it brings in the Cybersecurity aspect into consideration and also cross platform support as the later OPC DA only supports the Windows OS and not much of security to say be it 25K/50K tags.
Secondly, regarding some issues you are facing I'm not very clear on the exact problem you are facing with OFS. You should upgrade the OFS versions compatible with your SCADA.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-02-18 12:23 AM
I would suggest using OFSOPC for projects with a large amount of tags. The latest OFS versions no longer have the problems you are referring to. MODBUS (MODNET driver) is neither user friendly nor fast enough for large projects.
I have a project with 200k tags in 12 PLCs running via a single OFS server without problems.
The OPC/UA drivers in PlantSCADA are fairly new, so I have no information yet about performance or reliability. I would avoid them for now.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.