Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84488members
353708posts

smart 1000 ups battery test problem

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
dakotamar_apc
Cadet
0 Likes
1
58

smart 1000 ups battery test problem

This was originally posted on APC forums on 2/10/2011


Just recently replaced the batteries in this UPS with 12VDC 7Amp batteries (Yuasa - same rating of removed ones) and when the unit is tested the battery bar graph shows full bars for the test. two or three seconds after it finishes the test, the replace battery light will turn on and the unit will beep. If I test it again the unit will pass the test again and nothing else will happen, it will go back to normal operation.

What is causing this problem? The blades on the replacement batteries are smaller, is this causing problems?


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
58

Re: smart 1000 ups battery test problem

This reply was originally posted by Angela on APC forums on 2/10/2011


i dont know if it is but it is possible that one of the cells in those batteries is faulty. as an APC employee though, we cannot support third party batteries.

the UPS self test essentially compares the voltage drop of the batteries, while operating on battery, to a table stored in its memory to make sure the batteries are operating properly. If this test fails, then you'll see the replace battery LED come on.

other than trying a different batteries, i am not sure what else can be done. i have never seen this happen unless there is an issue with the batteries - faulty or maybe not fully charged? the batteries should be charged for at least 8 hours to ensure they are providing the expected results and runtime. during this time, you could turn the UPS off so that it is not being used or at least refrain from your own self tests.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
59

Re: smart 1000 ups battery test problem

This reply was originally posted by Angela on APC forums on 2/10/2011


i dont know if it is but it is possible that one of the cells in those batteries is faulty. as an APC employee though, we cannot support third party batteries.

the UPS self test essentially compares the voltage drop of the batteries, while operating on battery, to a table stored in its memory to make sure the batteries are operating properly. If this test fails, then you'll see the replace battery LED come on.

other than trying a different batteries, i am not sure what else can be done. i have never seen this happen unless there is an issue with the batteries - faulty or maybe not fully charged? the batteries should be charged for at least 8 hours to ensure they are providing the expected results and runtime. during this time, you could turn the UPS off so that it is not being used or at least refrain from your own self tests.