Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

existing UTS10BI adding an additional UTS6BI in parallel

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • existing UTS10BI adding an additional UTS6BI in parallel
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2151
Teken
Teken
154
Techie_apc
Techie_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2021-06-29 10:08 PM . Last Modified: ‎2024-03-20 03:15 AM

0 Likes
2
1391
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
Posted: ‎2021-06-29 10:08 PM . Last Modified: ‎2024-03-20 03:15 AM

existing UTS10BI adding an additional UTS6BI in parallel

I have an existing UTS10BI with the hard wired kit for a 50 amp generator. I have a 10,000 watt standby generator, can I add an additional UTS6BI to the feed from the generator?

Thanks for any help or assistance you can provide me.

Jimmac

Labels
  • Labels:
  • Universal Transfer Switch
  • Tags:
  • power
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Anonymous user
Not applicable

Posted: ‎2021-06-29 10:08 PM . Last Modified: ‎2024-03-20 03:14 AM

0 Likes
0
1391
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
Posted: ‎2021-06-29 10:08 PM . Last Modified: ‎2024-03-20 03:14 AM

Hi jimmac, the UTS unit are meant to be wired directly to a sub panel per electrical code. That being said if you have a way to wire the uts6bi to another panel and a have a way to get the generator output to it, then it could work. All of this is subject to local electrical code, so you might have to check on that as well. Hope this helps.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
Anonymous user
Not applicable

Posted: ‎2021-06-29 10:08 PM . Last Modified: ‎2024-03-20 03:14 AM

0 Likes
0
1391
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
Posted: ‎2021-06-29 10:08 PM . Last Modified: ‎2024-03-20 03:14 AM

Thanks for the response on this. I have now installed the second UTS on a sub-panel, when powering the UTS6BI from the sub-panel using a 20 amp two pole ganged breaker, and delivering 120V power on each of the two legs both "5 out" and "6 out"...the UTS will not power on? I metered out the spade lugs on the board both have 120V, but UTS will not power up? When I plug in a UPS to the UPS input, the UTS does power on and allow programming. Can you help me out with this one? I do have a call into tech support and a case number...but was cut off on the phone with a transfer to tech support.

Thanks,
Jim M

Reply

Link copied. Please paste this link to share this article on your social media post.

Anonymous user
Not applicable

Posted: ‎2021-06-29 10:08 PM . Last Modified: ‎2024-03-20 03:14 AM

0 Likes
0
1392
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
Posted: ‎2021-06-29 10:08 PM . Last Modified: ‎2024-03-20 03:14 AM

Hi jimmac, the UTS unit are meant to be wired directly to a sub panel per electrical code. That being said if you have a way to wire the uts6bi to another panel and a have a way to get the generator output to it, then it could work. All of this is subject to local electrical code, so you might have to check on that as well. Hope this helps.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.