Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84849members
354308posts

Update available for PC Business Edition Server

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
53

Update available for PC Business Edition Server

This question was originally posted by Max on APC forums on 10/30/2008


I'm now at the moment in a little trouble. We have a Server protected by a Smart UPS RT. Attached to the UPS was a CD with Powerchute Business Edition 6.6 which caused some well-known trouble. Meanwhile we installed a new version of the agent(i think it was 7.04.) During a planned reorganisation of the server, it was chosen to move the install drive of Powerchute to another disk drive. This is where my troubles started. First i uninstalled the agent and the server which didn't worked completely. Now i've got a few questions. Can you send me a how-to to deinstall the old version completely? Also i dont know in which way should i make the new installation. First the dowloaded agent(8.0), afterwards the server(6.6) from the cd? I'm thankfull for any kind of help, which can solve this troublesome situation. Please excuse my mistakes, i'm not a native speaker.


Accepted Solutions
EZ_Button_apc
Commander
Commander
0 Likes
0
53

Re: Update available for PC Business Edition Server

This was originally posted on APC forums on 10/30/2008


For the manual uninstallation instructions, give support a call at 800-890-4272.

As for the monitoring. If you use PCBE 8.0, the free version is just an agent. This agent does have an accessible web interface for your configuration needs. (http://:3052) Unless you have multiple agents to monitor, the server and console portions aren't that beneficial.

You can't use an old pcbe server version with a new agent, so certainly don't install version 6.x. In fact, probably toss that cd away just so you or anyone else uses it. 😃

See Answer In Context

1 Reply 1
EZ_Button_apc
Commander
Commander
0 Likes
0
54

Re: Update available for PC Business Edition Server

This was originally posted on APC forums on 10/30/2008


For the manual uninstallation instructions, give support a call at 800-890-4272.

As for the monitoring. If you use PCBE 8.0, the free version is just an agent. This agent does have an accessible web interface for your configuration needs. (http://:3052) Unless you have multiple agents to monitor, the server and console portions aren't that beneficial.

You can't use an old pcbe server version with a new agent, so certainly don't install version 6.x. In fact, probably toss that cd away just so you or anyone else uses it. 😃