Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Unable to install PowerChute Serial Shutdown software

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • Re: Unable to install PowerChute Serial Shutdown software
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2151
Teken
Teken
152
Techie_apc
Techie_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
atleast2characterslong
atleast2characterslong
Explorer

Posted: ‎2025-06-18 01:38 PM

0 Likes
2
2870
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
Posted: ‎2025-06-18 01:38 PM

Unable to install PowerChute Serial Shutdown software

I'm trying to install the software to use with a brand new APC Back-UPS 600. When I run the setup file, after accepting the terms, the setup doesn't do anything. It's still running in task manager. Here's what I get in the install log.

 

2025-06-18 15:44:25 --- Installing PowerChute Serial Shutdown 1.3.0.301
2025-06-18 15:44:25 --- .onInit
2025-06-18 15:44:27 --- CacheOSLanguage: OS language cached: 1033
2025-06-18 15:44:27 --- Setting up CommandLineConfigEditor tool
2025-06-18 15:44:27 --- CustomGUIInit
2025-06-18 15:44:27 --- PowerChute Serial Shutdown is not installed
2025-06-18 15:44:27 --- CheckJapaneseOS: OS language identifier detected: 1033
2025-06-18 15:44:27 --- Checking if PowerChute Business Edition is installed
2025-06-18 15:44:27 --- PowerChute Business Edition is not installed
2025-06-18 15:44:27 --- Microsoft Visual C++ 2017 Redistributable Package (x64) is already installed
2025-06-18 15:44:27 --- PowerChute Personal Edition is not installed
2025-06-18 15:44:32 --- UPS connected, checking hardware id before installing APCUPS driver
2025-06-18 15:44:33 Error installing APC NPM driver, return code -2

 

The device does show up under devices when I connect it to my computer. I also see the driver added to device manager. I've tried uninstalling the driver before attempting the install again which does not help. Nor does updating the driver in the device manager. I've also tried restarting the computer and the UPS as well as trying to install without it plugged in.

 

Any other ideas why the setup could be getting stuck?

Labels
  • Labels:
  • Home & Office - UPS & Software
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
fredkm
fredkm Troubleshooter
Troubleshooter

Posted: ‎2025-06-19 10:59 PM

1 Like
1
2855
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
Posted: ‎2025-06-19 10:59 PM

PowerChute Serial Shutdown installs a so called null-driver (named 'APC UPS') which replaces the plug-and-play driver (named 'HID UPS Battery'). The purpose of the null-driver is disabling native power management on the OS for the UPS. I.e. you want PowerChute Serial Shutdown to protect your computer during power failures, and you don't want a Windows power plan interfering with this.

 

From the installation logs I can see that null-driver installation fails. This will occur if there is no UPS connected to a USB port during installation. Obviously that's not the case for you as you state you have the UPS connected. Error code -2 means the hardware ID of your UPS did not match any of the known APC UPS hardware IDs. Not sure why the installer hangs at this point.

 

Some things you could try:

- Make sure you've got latest Windows updates installed (early Win 11 versions had issues with USB devices).

- Try a different USB port.

 

If it doesn't work then could you please provide some additional information to help us troubleshooting your issue:

  • Your UPS model which you can find on sticker at the back or bottom of the UPS (it should be different from the generic 'Back-UPS 600' name you already provided).
  • Your Windows version and build.
  • The UPS hardware Id. You can find this through 'Control Panel - Device Manager'. Right-click the 'HID UPS Battery' device and select  'Properties' from the context menu. Open 'Details' tab and in the dropdown select 'Hardware Ids'
    fredkm_0-1750398947115.png

     

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
fredkm
fredkm Troubleshooter
Troubleshooter

Posted: ‎2025-06-19 10:59 PM

1 Like
1
2856
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
Posted: ‎2025-06-19 10:59 PM

PowerChute Serial Shutdown installs a so called null-driver (named 'APC UPS') which replaces the plug-and-play driver (named 'HID UPS Battery'). The purpose of the null-driver is disabling native power management on the OS for the UPS. I.e. you want PowerChute Serial Shutdown to protect your computer during power failures, and you don't want a Windows power plan interfering with this.

 

From the installation logs I can see that null-driver installation fails. This will occur if there is no UPS connected to a USB port during installation. Obviously that's not the case for you as you state you have the UPS connected. Error code -2 means the hardware ID of your UPS did not match any of the known APC UPS hardware IDs. Not sure why the installer hangs at this point.

 

Some things you could try:

- Make sure you've got latest Windows updates installed (early Win 11 versions had issues with USB devices).

- Try a different USB port.

 

If it doesn't work then could you please provide some additional information to help us troubleshooting your issue:

  • Your UPS model which you can find on sticker at the back or bottom of the UPS (it should be different from the generic 'Back-UPS 600' name you already provided).
  • Your Windows version and build.
  • The UPS hardware Id. You can find this through 'Control Panel - Device Manager'. Right-click the 'HID UPS Battery' device and select  'Properties' from the context menu. Open 'Details' tab and in the dropdown select 'Hardware Ids'
    fredkm_0-1750398947115.png

     

Reply

Link copied. Please paste this link to share this article on your social media post.

atleast2characterslong
atleast2characterslong
Explorer

Posted: ‎2025-06-27 05:25 AM

In response to fredkm
1 Like
0
2776
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
Posted: ‎2025-06-27 05:25 AM

I was able to install it on a different computer without an issue. I still have not been able to install it on my computer, but since this UPC was purchased for a coworker's computer and it is working, I am not going to try and further diagnose the problem. I appreciate the quick and detailed response. Thanks for your help.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.