Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84725members
354138posts

USB Cable 940-0127E vs 940-0127A/B

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
nikolay_zhelev_apc
Ensign
Ensign
0 Likes
2
845

USB Cable 940-0127E vs 940-0127A/B

This was originally posted on APC forums on 11/10/2014


Dear APC Team,

I have couple of questions regarding the cable 940-0127E FCI.

1. Is that simple or smart cable?

2. What is the difference between 940-0127E and 940-0127A/B cable?

3. What means FCI at the end of the P/N?

4. Is that a pure USB cabe or it's RS232 cable with USB connector?

I'm using UPS BR550GI.

I'm looking forward to hearing from you!

Sincerely Yours,

Nikolay Zhelev


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
845

Re: USB Cable 940-0127E vs 940-0127A/B

This reply was originally posted by Angela on APC forums on 11/10/2014


Hi,

What I know is:

  • Some places reference this as a simple cable but I think it has both simple/smart applications. For this UPS, it is a smart cable/communication - meaning two way communication between UPS and the computer (or whatever you connect it to). Simple is what we call a one way communication cable - from the UPS to something else. This application is smart in the sense you can issue commands, read information, change settings, etc.
  • We change the letter on the cables to identify the revision. When we change it, it is usually because we changed a connector, vendor we use, color, etc. If the part number remains the same, then it has the same functionality.
  • FCI is the vendor that makes the cables. As a general strategy, many of our parts/cables are sourced from more than one vendor and we ensure the functionality remains the same, in case there is a problem sourcing parts from a single vendor.
  • This is a standard USB cable with a keyed RJ-45 connection

See Answer In Context

nikolay_zhelev_apc
Ensign
Ensign
0 Likes
0
846

Re: USB Cable 940-0127E vs 940-0127A/B

This was originally posted on APC forums on 11/10/2014


Hi Angela,

Thank you very much for this complete answer!

Kind Regards,

Nikolay Zhelev

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
846

Re: USB Cable 940-0127E vs 940-0127A/B

This reply was originally posted by Angela on APC forums on 11/10/2014


Hi,

What I know is:

  • Some places reference this as a simple cable but I think it has both simple/smart applications. For this UPS, it is a smart cable/communication - meaning two way communication between UPS and the computer (or whatever you connect it to). Simple is what we call a one way communication cable - from the UPS to something else. This application is smart in the sense you can issue commands, read information, change settings, etc.
  • We change the letter on the cables to identify the revision. When we change it, it is usually because we changed a connector, vendor we use, color, etc. If the part number remains the same, then it has the same functionality.
  • FCI is the vendor that makes the cables. As a general strategy, many of our parts/cables are sourced from more than one vendor and we ensure the functionality remains the same, in case there is a problem sourcing parts from a single vendor.
  • This is a standard USB cable with a keyed RJ-45 connection

nikolay_zhelev_apc
Ensign
Ensign
0 Likes
0
847

Re: USB Cable 940-0127E vs 940-0127A/B

This was originally posted on APC forums on 11/10/2014


Hi Angela,

Thank you very much for this complete answer!

Kind Regards,

Nikolay Zhelev