Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

UPC2200 SMT2200I forcing to online for audio

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • Re: UPC2200 SMT2200I forcing to online for audio
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2150
Teken
Teken
144
Techie_apc
Techie_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
claudiomas
claudiomas
Explorer

Posted: ‎2024-09-04 02:13 AM

0 Likes
2
657
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
Posted: ‎2024-09-04 02:13 AM

UPC2200 SMT2200I forcing to online for audio

hello i need pure sinewave main supply for HiEnd audio application, so how to configure the UPC for rebuilt clean  online 230/240V output supply and keep the main dirty high THD 240V  supply only for charging battery ??? i'm electronic service engineer so i can do the job, used to high voltage up to 1K2V tube amplifier, thanks for your advise

Labels
  • Labels:
  • Home & Office - UPS & Software
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
Teken
Teken
Champion

Posted: ‎2024-09-06 08:01 AM . Last Modified: ‎2024-09-06 08:03 AM

0 Likes
0
620
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
Posted: ‎2024-09-06 08:01 AM . Last Modified: ‎2024-09-06 08:03 AM

I’m going to have to ask you to explain this a little better as I am not quite clear as to what the question is?!? 🤔

 

Regardless, the SMT2200I is a Line Interactive Pure Sine Wave UPS. As such there is nothing required to obtain a pure sine wave if the audio equipment is connected to the UPS outputs. ☝️

 

If and when there is a lights out / grid down event when the system goes into battery only mode.

 

The output voltage will also be a pure sine wave. 

 

The system incorporates various RFI / EMI filters to reduce such interference. The system incorporates an AVR circuit that can be adjusted for upper / lower input transfer voltage which allows a wider range of AC voltage to be accepted if desired.

 

Lastly, the system has a power quality control system that allows the system to accept so called dirty power which can be adjusted if required.

 

The power quality setting is directly related to input voltage, frequency, slew rate, THD. Any fast transients on input voltage are also detected by this circuit.

 

NOTE: The average service life of the battery is 2-5 years based on usage, temperature, and environmental conditions. Forcing the system to be more sensitive and going into battery only mode will reduce the operational service life which translates to more long term costs. 

Reply

Link copied. Please paste this link to share this article on your social media post.

claudiomas
claudiomas
Explorer

Posted: ‎2024-09-07 12:19 AM

0 Likes
0
586
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
Posted: ‎2024-09-07 12:19 AM

helo, thanks for questions,  output voltage its a pure sine wave only on battery mode, for evening audio session i need 4/5Heures autonomy,  so of course to multiply battery can be a solution , or better external smps 24V 600W+ internal battery, i think the two 24V battery are in parallel mode  so can i shunt thems
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.