Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the Schneider Electric Community! We have moved to a new address: community.se.com — bookmark it today and contact SchneiderCommunity.Support@se.com if you have any questions!
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82639members
350287posts

Software Question - Back-UPS CS 350 & Ativa AT-BU 1200

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
mikey5555_apc
Cadet
0 Likes
2
186

Software Question - Back-UPS CS 350 & Ativa AT-BU 1200

This was originally posted on APC forums on 8/17/2009


Hello all,
I am in need of software for monitoring the UPS and shutting down the PCs running Linux. Actually, the OSs are UBUNTU 9.10 (my desktop PC) and CentOS 5 (My very small Web Server - only 6 domains).
I see a choice for Linux in the Software Download pages for PowerChute Business Edition 8.0.1 - Single Node Agent.
Will this software version work for both CentOS (32 bit OS) and UBUNTU (64 bit OS)?
Is there a better choice?
Any advice or pointers are greatly appreciated...

mikey5555


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
186

Re: Software Question - Back-UPS CS 350 & Ativa AT-BU 1200

This reply was originally posted by Jonathan on APC forums on 8/17/2009


Welcome to the APC Forum Mike.

If you are using our Back-UPS product line the software that comes with it is the PowerChute Personal Edition. Our PCPE software is designed to work with Microsoft based computers and Mac OS 10.3.9 up to 10.4.1.

Our PowerChute Business Edition is designed for higher level UPSs such as our Smart-UPS. PCBE as well call it, is tested to work with Red Hat and SuSE Linux. You can see the supported Operating System by clicking on this link --> [PCBE Compatibility Guide|http://www.apcmedia.com/salestools/ASTE-6Z5QEV_R10_EN.pdf]

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
186

Re: Software Question - Back-UPS CS 350 & Ativa AT-BU 1200

This reply was originally posted by Angela on APC forums on 8/17/2009


you could look into apcupsd which is a third party software but has the ability to monitor these UPSs. i have also heard of NUT as well.

APC does not have software for use with the Back UPS family on Linux at this time.

i attached the users manual for apcupsd.

Attachments
BillP
Administrator Administrator
Administrator
0 Likes
0
187

Re: Software Question - Back-UPS CS 350 & Ativa AT-BU 1200

This reply was originally posted by Jonathan on APC forums on 8/17/2009


Welcome to the APC Forum Mike.

If you are using our Back-UPS product line the software that comes with it is the PowerChute Personal Edition. Our PCPE software is designed to work with Microsoft based computers and Mac OS 10.3.9 up to 10.4.1.

Our PowerChute Business Edition is designed for higher level UPSs such as our Smart-UPS. PCBE as well call it, is tested to work with Red Hat and SuSE Linux. You can see the supported Operating System by clicking on this link --> [PCBE Compatibility Guide|http://www.apcmedia.com/salestools/ASTE-6Z5QEV_R10_EN.pdf]