Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84471members
353689posts

Powerchute and Win 7 Power options

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
homer_at_apc
Cadet
0 Likes
2
73

Powerchute and Win 7 Power options

This was originally posted on APC forums on 1/7/2012


I have a new Br1000G which I like. I first connected the USB cable without the Powerchute software installed. Drivers were automatically loaded and I think this added battery options to the Win7 power options, so I set up Win7 to alarm and shut down when on UPS battery.

I then installed Powerchute, which removed the Win7 battery options. Powerchute is ok, but I don't like the moderate file it loads into RAM, and multiple services it loads. So I removed Powerchute and Win 7 battery options were NOT restored.

?? How do I turn win 7 battery options back on?

I would like to run Powerchute periodically on request to view power use and set options like slaved outlets. Is there a lite version or web browser based version I can run occasionally, but still let Win 7 power options control shutdown after switching to battery?

thanks
homer


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
74

Re: Powerchute and Win 7 Power options

This reply was originally posted by Jonathan on APC forums on 1/10/2012


Hi Homer,

Unfortunately we do not have any Lite or web version of PowerChute Personal. From my experience, in order for you to use PowerChute Personal the APC UPS should be detected as APC UPS under device manager. In the event that you would like to revert back to the Windows 7 Native UPS application you would then need to update/uninstall the APC UPS and have it detected as HID UPS Battery. Once it is set to HID UPS Battery it should display back the Native Battery Option setting.

See Answer In Context

2 Replies 2
homer_at_apc
Cadet
0 Likes
0
74

Re: Powerchute and Win 7 Power options

This was originally posted on APC forums on 1/10/2012


JonPro- Thanks for answering my questions. I will use your procedure in the future. I am also going to try the Try and Decide option in Acronis True Image to load PowerChute for awhile - then revert back.

homer_at

BillP
Administrator Administrator
Administrator
0 Likes
0
75

Re: Powerchute and Win 7 Power options

This reply was originally posted by Jonathan on APC forums on 1/10/2012


Hi Homer,

Unfortunately we do not have any Lite or web version of PowerChute Personal. From my experience, in order for you to use PowerChute Personal the APC UPS should be detected as APC UPS under device manager. In the event that you would like to revert back to the Windows 7 Native UPS application you would then need to update/uninstall the APC UPS and have it detected as HID UPS Battery. Once it is set to HID UPS Battery it should display back the Native Battery Option setting.