Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84757members
354189posts

PowerChute/Back-UPS RS 800 reports bad AC voltage, but AC voltage is just fine. Is this a circuitry or battery problem?

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
dwwheelock_apc
Cadet
0 Likes
1
129

PowerChute/Back-UPS RS 800 reports bad AC voltage, but AC voltage is just fine. Is this a circuitry or battery problem?

This was originally posted on APC forums on 10/15/2013


I have a Back-UPS RS 800 that we received in 2004.  We have replaced the battery in the past and the current battery is about 3 years old. 

Currently, this unit is repeatedly switching to battery for a fraction of a second, often many times in a single minute, but sometimes not for many minutes.  When I check the status in PowerChute, it reports that the UPS says that the the line AC voltage is varying wildly, high and low.  However, I have tested the line AC voltage and there is nothing wrong with it.  The AC voltage is rock-steady at 122 volts.

When I use PowerChute to run a battery Self_Test it says that the battery is bad.  However, when I test the UPS by simply unplugging it from the wall, then PowerChute accurately predicts that the battery will power the computer for about 10 minutes.  When I plug it back in after about 5 minutes, it still reports about 5 minutes of runtime remaining .  So, in terms of runtime, the battery is working just fine.

The UPS has also occasionally freaked out and cut off power the computer a few times in the last few weeks.  The unit is not overloaded and only has one computer and dual-monitors connected.  It has powered this same computer and monitors for many years.

So the question here is symptoms.  The UPS/PowerChute report bad AC line voltage when the voltage is just fine.  AND the UPS/PowerChute report that the 3-year-old battery is bad, but the battery still has plenty of runtime left.  AND the UPS is cutting power sporadically.

Questions:

Is this a circuitry problem in the UPS or can a battery cause this symptoms? 

Is it just time to replace this UPS?


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
129

Re: PowerChute/Back-UPS RS 800 reports bad AC voltage, but AC voltage is just fine. Is this a circuitry or battery problem?

This reply was originally posted by Bill on APC forums on 10/15/2013


Hi,

Since the UPS is 9 years old and the battery is 3 years old I suggest replacing the unit. You can take advantage of the Trade UPS program where you trade in your old UPS and receive a discount on a new one.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
130

Re: PowerChute/Back-UPS RS 800 reports bad AC voltage, but AC voltage is just fine. Is this a circuitry or battery problem?

This reply was originally posted by Bill on APC forums on 10/15/2013


Hi,

Since the UPS is 9 years old and the battery is 3 years old I suggest replacing the unit. You can take advantage of the Trade UPS program where you trade in your old UPS and receive a discount on a new one.