Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84541members
353794posts

PC Reboots by itself with APC UPS Model BR1000IN

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
custardapple_apc
Cadet
0 Likes
1
60

PC Reboots by itself with APC UPS Model BR1000IN

This was originally posted on APC forums on 8/3/2011


I bought a new APC UPS RS 1000 (*Model BR1000IN*) and have been using it. The PC reboots by itself at irregular intervals, and this problem exists ever since I started using this UPS. I have connected only my PC, 18” TFT monitor and the modem to the UPS.

The problem of the PC rebooting itself was not there when I was using APC UPS 500 (*Model BP500I*). I have now switched back to APC UPS 500, with the same load as above, and the PC is not rebooting. But this UPS gives a battery backup of only about 20 minutes.

My computer has a Celeron CPU, 900 MHz, 1.20 GHz, 384 MB RAM. OS is Windows XP SP3.

I checked for virus and spyware and tested the memory and the results came out clean.

Please help to resolve the problem. Thank you in advance.

Message was edited by: custardapple


Accepted Solutions
Techie_apc
Admiral
Admiral
0 Likes
0
60

Re: PC Reboots by itself with APC UPS Model BR1000IN

This was originally posted on APC forums on 8/5/2011


my suggestion is to check whether the PC power cord is connected to the surge only outlet or battery backup outlet. if it is connected to surge only outlet, then pls switch over to battery backup outlet and then check whether the problem persists or not. if the problem persists, then pls call India Customer Care Center at 1-800-4254-272/472 for onsite engineer visit.

See Answer In Context

1 Reply 1
Techie_apc
Admiral
Admiral
0 Likes
0
61

Re: PC Reboots by itself with APC UPS Model BR1000IN

This was originally posted on APC forums on 8/5/2011


my suggestion is to check whether the PC power cord is connected to the surge only outlet or battery backup outlet. if it is connected to surge only outlet, then pls switch over to battery backup outlet and then check whether the problem persists or not. if the problem persists, then pls call India Customer Care Center at 1-800-4254-272/472 for onsite engineer visit.