Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84528members
353773posts

New APC Model BR800blk

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
cathudog_apc
Lieutenant JG
Lieutenant JG
0 Likes
12
558

New APC Model BR800blk

This was originally posted on APC forums on 3/14/2008


I got this new unit and it switches to go on battery more often then other old G model or the BB model 11 times since put on line 24 hours ago and the alerts are all blackouts is this normal. I have no USB connection problems thank God.


Accepted Solutions
cathudog_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 4/21/2008


Thanks i have the alarm off so i do not hear only the clicks at the unit I will leave it on default or next time I shut down try the low setting thanks NK for the fast response hope you had a good vacation or time off.

See Answer In Context

12 Replies 12
TheNotoriousKMP_apc
Sisko
Sisko
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 3/14/2008


Chris,

I apologize for the frustration you're receiving across the board with these two products. Is the sensitivity on the RS800 already set to low? Does the software record any type of electrical noise? Is the UPS on the same circuit as any other large appliance?

cathudog_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 3/14/2008


No electrical noise tried letting to low, the only thing I can think is it's because the fluctuation in voltage around here, and this unit has has the feature to monitor voltage and it is going on battery because of that, because I have read if the voltage start to go up or down the APC doesn't now how high or low it is going to go so it will go on battery ( tell me if I am wrong on this one) 9 times in 24 hours 14 total since on line and all registered as blackout. The system is on a brand new circuit just for this system except of av receiver and TV that is all thats on this circuit. The only thing plugged into the APC is the tower nothing else and it says it is using 145 watts and the other G model read it as 97 watts if that matters. I love this unit and I guess this is the way it is going to work.

TheNotoriousKMP_apc
Sisko
Sisko
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 3/15/2008


Did you adjust the voltage transfer points to increase the ability for AVR instead of forcing it on battery?

Based on your power problems, you may be right. The UPS may finally be doing what you've wanted it to.

cathudog_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 3/15/2008


I set it to high I might have to set it back to medium if I keep getting a lot of battery switches but haven't had one in quite a while it is working as it should as far as i know and I am quite happy with this unit and APC customer service give then an A+. Thanks for your help

TheNotoriousKMP_apc
Sisko
Sisko
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 3/24/2008


Haha. I clearly didn't ponder what this would do and just decided to do it with an RS1500LCD. It immediately flatlined and gave me an F6. The tone wouldn't stop until I disconnected the battery.

My recommendation? I'd stay away from it.

SaGeUvAgOnY_apc
Ensign
Ensign
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 3/24/2008


I just received my BR800BLK today, and not one single hiccup or error so far. No more crazy pop ups! Does it feel nice now that it doesn't nag about communications errors? * slowly falls asleep since it's so quiet without the notifications now *

THANK YOU KEVIN!!!!


Ohh and one weird question, what happens when you plug a UPS into itself in the battery backup port? Not something I'd ever dare try, but as I was packaging the BE750G away, I asked myself that question..

cathudog_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 3/26/2008


I put my sensitivity back to default the yellow and red light lite on the front and now i hardly have any beeps but up until know I have had 141 thats the power around here. Very pleased with this unit may have to upgrade my others to a unit like this but I need a BB like version so i can hook the cable model to the APC for added protection any suggestion NK

TheNotoriousKMP_apc
Sisko
Sisko
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 3/26/2008


Christy,

If you're using a broadband/cable modem, you should still have adequate surge protection. The feeling that APC had with signal loss over coax was removed on our new LCD's, and left with Cat5 surge only. So in essence, you can put the Cat5 line from the cable modem through the RS800BLK, then out to either a router or your home machine, and still have the surge protection. For actual coax protection, you would need to have something like the PV (http://www.apc.com/resource/include/techspec_index.cfm?base_sku=PV).

cathudog_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 3/26/2008


I have my 750 BB and the 700BB both with the cable going through it and see no loss of signal but that just me some other might of saw some loss of signal so that is no longer an option and yes I am using the Ethernet or RJ-45 through the BR800BLK also on my APC's. Thanks once again for your info wish all CSReps were as good as you.

cathudog_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 4/21/2008


I have the new APC set at the default front AVP setting and I am getting 12 blackout a day due to voltage fluctuation's will this wear out the unit prematurely or should i lower the setting to the lowest setting on the lights on the front. Transfer voltage and sensitivity adjustment is what I am talking about or is the unit not operating properly I thought setting it too the default position what stop some of the going on battery tripes and it did but still get about 12 a day around 4am 9am 4pm 6pm are about when the tripes occur.

TheNotoriousKMP_apc
Sisko
Sisko
0 Likes
0
558

Re: New APC Model BR800blk

This was originally posted on APC forums on 4/21/2008


If there's a voltage fluctuation, that will force the UPS on battery regardless of what the settings are, as it means one of the reasons why a UPS will transfer to battery (change in voltage / change in time). However, if the voltage fluctuates, and remains at that voltage for a sustained period of time, feel free to adjust the sensitivty to low.

cathudog_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
559

Re: New APC Model BR800blk

This was originally posted on APC forums on 4/21/2008


Thanks i have the alarm off so i do not hear only the clicks at the unit I will leave it on default or next time I shut down try the low setting thanks NK for the fast response hope you had a good vacation or time off.