Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84581members
353849posts

Getting a UPS need some info on graceful shutdowns.

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
shawshank_apc
Cadet
0 Likes
2
131

Getting a UPS need some info on graceful shutdowns.

This was originally posted on APC forums on 4/12/2011


Hi all,

I am getting a UPS for 3 devices I have in a small rack.

I was wondering, does the Back-UPS Pro series do a graceful shutdown to all connected devices once there is a power failure?
I was unable to find what I need from the website.

Thanks in advance!!!


Accepted Solutions
pfoomer_apc
Ensign
Ensign
0 Likes
0
131

Re: Getting a UPS need some info on graceful shutdowns.

This was originally posted on APC forums on 4/13/2011


Hi

yes this can be achieved, by running daemons on the non connected to the ups computers, and getting the connected ups computer to send a message to initiate shutdown.

I do this from my mac, to shutdown down my nas.

Modifications to both systems scripts were required, its not easy, but it is possible ( and free!!)

Perhaps you can provide more information on what is connected to the ups, and what you want to shutdown.

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
132

Re: Getting a UPS need some info on graceful shutdowns.

This reply was originally posted by Angela on APC forums on 4/13/2011


any Back UPS can only shutdown one attached client via USB - it can do this via Powerchute personal edition and a supported operating system or if the native OS as built in support.

If you need to shutdown multiple clients gracefully, you'll want to take a look at these (more pricier) options: Referenced content removed

do all of these clients require a graceful, unattended shutdown? if not, then you can just plug them in and then the UPS will turn off when it exhausts it battery and cut output power. i couldnt tell based on your initial question if you required a graceful shutdown.

pfoomer_apc
Ensign
Ensign
0 Likes
0
132

Re: Getting a UPS need some info on graceful shutdowns.

This was originally posted on APC forums on 4/13/2011


Hi

yes this can be achieved, by running daemons on the non connected to the ups computers, and getting the connected ups computer to send a message to initiate shutdown.

I do this from my mac, to shutdown down my nas.

Modifications to both systems scripts were required, its not easy, but it is possible ( and free!!)

Perhaps you can provide more information on what is connected to the ups, and what you want to shutdown.