Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Search in
Posted: 2022-07-14 04:44 AM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-07-14 04:44 AM
Hi,
when I saw the problems with the batteries I thought it would also be the right time to update firmwares.
One UPS got a AP9630 and the other a AP9631. Both seem to have the same firmware file named "apc_hw05_aos708_sumx708_bootmon109.exe". Currently we are still running SUMX 6.5.0, AOS 6.5.0 and Boot Monitor 1.0.8 on both of them.
When I run the upgrade utility I get these messages on both UPS:
[Date-Time] Unable to update device IP with Boot Monitor, stopping all further processing of this device!
[Date-Time] Uploading firmware file 1 of 3: Boot Monitor to IP, please wait...
[Date-Time] Firmware distribution does not match target device platform; this could be due to a corrupt distribution.
[Date-Time] NMC Firmware Update Utility v1.0.4 initialized.
Am I using the wrong firmware version? This is the version that I found and I believe that this is for a AP9630 in a SMT3000RMI2U and a AP9631 in a SMX3000RMHV2U (web site said it is for Smart-UPS and Galaxy 3500). Am I wrong? What else might have happend here?
The firmware for the SMX3000RMHV2U is UPS 07.4 (ID1003) and for the SMT3000RMI2U it is UPS 09.3 (ID18). Are these the actual versions or should I upgrade these, too? Where do I get updated firmware from? I did not find any.
Thanks a lot!
pompfe
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-07-26 12:20 PM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-07-26 12:20 PM
After comparing configs, I found it was because the protocol selected for updates was disabled on device in question. After switching the protocol (or enabling the protocol in the NMC2) the updates proceeded. Make sure you have FTP/SCP connectivity using an external client or checking the config before trying the update utility. Hope this helps.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-07-26 12:13 PM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-07-26 12:13 PM
I have the same issue but across 20 UPS I only have 3 or 4 that have the issue. They are the same model and hardware revision (AP9630) and I'm using apc_hw05_aos708_sumx708_bootmon109) and some can update and others cannot. Very strange. Did you find a solution?
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-07-26 12:20 PM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-07-26 12:20 PM
After comparing configs, I found it was because the protocol selected for updates was disabled on device in question. After switching the protocol (or enabling the protocol in the NMC2) the updates proceeded. Make sure you have FTP/SCP connectivity using an external client or checking the config before trying the update utility. Hope this helps.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-02-08 04:36 AM
Yes, this is exactly what it was for me - SSH was disabled. Thank you!
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-08-03 06:34 PM
I discovered that my APC PD8841 was outdated to the point that I needed to configure my SSH settings to use specific ciphers and key exchange algorithms for the firmware update tool to work correctly. Follow the steps below to determine if this issue affects you.
1. Attempt to SSH into the APC unit with SSH enabled on the device:
ssh apc@IP_OF_DEVICE
2. If you receive an error like "no matching key exchange method found. Their offer: diffie-hellman-group-exchange-sha1,diffie-hellman-group1-sha1" add one of the key exchange algorithms offered to your SSH command and try again:
ssh -o KexAlgorithms=+diffie-hellman-group1-sha1 apc@IP_OF_DEVICE
NOTE: If you do not receive an error and instead see a password prompt or an option to add the device fingerprint to your known_hosts, this solution may not resolve your issue.
3. If you then receive another error stating "no matching cipher found. Their offer: aes256-cbc,3des-cbc,blowfish-cbc,arcfour" add one of the ciphers offered to your SSH command and try again. Otherwise, skip to step 4:
ssh -o KexAlgorithms=+diffie-hellman-group1-sha1 -c aes256-cbc apc@IP_OF_DEVICE
4. You should now be able to SSH into the device. If successful, create an SSH configuration file named config with no file extension in your user folder $HOME\.ssh. This example assumes you are using Windows, but the process is similar on Linux:
Host IP_OF_DEVICE
KexAlgorithms +diffie-hellman-group1-sha1
Ciphers aes256-cbc
NOTE: Ensure the file has no file extension; otherwise, SSH will not recognize it. To confirm, open a terminal in the .ssh folder and list the files using ls or dir, depending on your OS.
5. Open a new terminal and try to SSH into the device without using any command line arguments. If your SSH configuration file is recognized, you should be able to connect without specifying additional options. If successful, proceed to step 6. If not, further troubleshooting is required:
ssh apc@IP_OF_DEVICE
6. With SSH now automatically using these options for your device, try the firmware update utility again. You should now be able to update the firmware.
7. After updating the firmware, it is highly recommended that you remove the SSH configuration for this device by deleting the SSH configuration options or file you created in the steps above. If you decide not to remove this, you will continue using outdated ciphers and key exchange algorithms, which pose a security concern.
8. The new firmware should now accept the default secure key exchange algorithms and ciphers. To test this, try to SSH into the device again using the standard command with the custom options for this device removed from the SSH configuration file:
ssh apc@IP_OF_DEVICE
NOTE: If you still encounter key exchange or cipher errors, the device will still require the custom SSH configuration options until another firmware update adds support for them.
I hope this helps someone else who encounters a similarly outdated APC unit.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-06-27 03:50 AM
Hello,
i had the same problem. Searched 3 days. No help from the hotline. They just told me this solution posibility here in the user forum. Thats support of a premium manufacturer. Holy...
My Solution was, to use the only the superuser "apc", not selfmade users, even if they are with administration right. The Failure messages are completly wrong and missleading in my case.
A simple hint in the software itself, could save ours of peoples life. "Only use Superuser apc for the Updates". I hate this kind of sloppiness in the complete IT.
I hope it helps someone and saves time.
Best regards,
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-21 08:20 AM
I found that the best way to upgrade the AP9630 is via CONSOLE cable. APC has a official documentation or just search TubeYou "Recovering & Uploading Firmware on APC Network Management Card 2 | Schneider Electric Support". It works even with bricked card. Console updating process ,worked for me everytime.
NMC Firmware Update Utility bricked every AP9630 which I tried to update. Even though I downloaded NMC FUU straight from the official webpage i.e. APC_SUMX_EN-7.2.2.zip for APC SmartUPS SMT750IC
. If the NMC FUU complains about "Firmware distribution does not match target device platform" DO NOT CONTINUE THE UPDATE PROCESS IF you don't have console cable at hand or the card is at remote location.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.