Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84541members
353794posts

Can a UPS sit around unused?

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
Dave2001_apc
Crewman
Crewman
0 Likes
3
336

Can a UPS sit around unused?

This was originally posted on APC forums on 11/5/2008


I am needing to have an extra UPS around to keep some equipment up and running for when the batteries fail. What happens to the batteries if they sit unused? Should I rotate the UPS in and out of service?
Thanks.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
336

Re: Can a UPS sit around unused?

This reply was originally posted by Matt on APC forums on 12/20/2008


Also it is best practice to store the batteries close to 20C and disconnected from the UPS. Some UPSs, such as Smart-UPS, can actively drain the batteries while unplugged to run their internal logic systems.

See Answer In Context

3 Replies 3
Richard_FDisk_apc
Ensign
Ensign
0 Likes
0
336

Re: Can a UPS sit around unused?

This was originally posted on APC forums on 11/6/2008


Hello;

The batteries will go dead over time and if they sit dead too long they can become unusable
(Just ask anyone who's ever bought a used car that sat for a really long time and had to get a new battery for it)

it's best to keep it at least plugged in to keep a charge on the battery packs

cheers

rau_apc
Commander
Commander
0 Likes
0
336

Re: Can a UPS sit around unused?

This was originally posted on APC forums on 11/6/2008


If batteries are kept unused for too long, let's say, one year without being charged from time to time, it will possible get worn out. If you need to keep the unit unused, at least plug it to the wall outlet for 12 to 16 hours every 3 to 6 months. Even so, the batteries are still getting old as the months pass, it will eventually get useless after a few years.

If the temperature where the batteries are kept is too high or too low, the batteries will wear out quicker. Keep them at 15 to 25C.

BillP
Administrator Administrator
Administrator
0 Likes
0
337

Re: Can a UPS sit around unused?

This reply was originally posted by Matt on APC forums on 12/20/2008


Also it is best practice to store the batteries close to 20C and disconnected from the UPS. Some UPSs, such as Smart-UPS, can actively drain the batteries while unplugged to run their internal logic systems.