Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
It's your place to connect with experts and peers, get continuous support, and share knowledge.
Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-29 05:20 AM
This was originally posted on APC forums on 1/21/2011
I have a Back-UPS Pro 1000 (BR1000G) that I would like to use with a Windows Server 2008 machine (communicating via USB cable). It's a Dell PowerEdge server, although that probably makes little difference, and I'm running the 64-bit version of Windows 2008 Server, which may make a difference). However, it appears that APC does not intend for their customers to use any of their "Back-UPS" products to protect server hardware, and they are not marketed for that purpose.
From what I've researched and been told by APC support, PowerChute Business Edition (which I installed) works with Windows Server 2008, but it does not support monitoring of their "Back-UPS" units. PowerChute Personal Edition will support their "Back-UPS" units, but it is not guaranteed to work on Windows Server 2008, and APC will not support its use on that OS.
Does anyone have experience using PCPE on a Windows 2008 Server ? Will PCPE install and reliably shut down the server during a power outage ?
Thank You !
Message was edited by: SineWave
Posted: 2021-06-29 05:20 AM
This reply was originally posted by Angela on APC forums on 1/27/2011
Posted: 2021-06-29 05:20 AM
This reply was originally posted by Angela on APC forums on 1/21/2011
PCPE is not recommended to be installed on Server 2008. Server OSs are generally designed to user Server Type UPSs, like a Smart UPS or Symmetra LX. They do indeed utilize PowerChute Business Edition versus Back UPS that utilize PowerChute Personal Edition.
I understand that there are other computers out there though using Server OSs but do not require a Smart UPS.
Ultimately, Server 2008 will not be supported by APC for use with PCPE. It is not on the compatibility chart and you may run into issues installing/uninstalling it. I would recommend against it but for your application it may work.
PCPE compatibility chart -> http://www.apcmedia.com/salestools/JNOE-7GSAQJ_R8_EN.pdf
Posted: 2021-06-29 05:20 AM
This was originally posted on APC forums on 1/22/2011
Thank you, picKed, (who responded)... "PCPE is not recommended to be installed on Server 2008"
Yes, that was my understanding also, but I was hoping to hear other people's experience, such as "I could not get it to work no matter what I tried", or perhaps someone replying with something like "It's not officially supported, but it should work just fine... I've had personal edition running on my Win Server 2008 box for a year now without any problems", or something similar.
I guess I'll attempt to install PCPE on my server and see what happens. It's a brand new system with no production stuff running on it yet, so even if something horrific should happen, like the server hanging or failing to shutdown during an outage, no big deal. Besides, I like adventure.
(If this message board lets me quote a previous post in my reply, I can't figure out how to do it.)
Message was edited by: SineWave
Posted: 2021-06-29 05:20 AM
This reply was originally posted by Angela on APC forums on 1/24/2011
alrighty. i agree with clarkson here. many people ask for the manual uninstall instructions after botched installs. i have seen a small success rate on server *2003* but not really with 2008.
Posted: 2021-06-29 05:20 AM
This was originally posted on APC forums on 1/27/2011
Well, I did install Powerchute Personal Edition 3.0 for Windows 7 (although I don't know if the PCPE 3.0 downloads for Vista, XP, etc on APCs website are in fact different than the one labeled specifically for Win 7) on my Windows 2008 Server (64-bit) before I read the advice against doing so fron Clarkson & PicKed.
It installed without any obvious problems, and it appears to be functioning correctly. It displays correct status info for the UPS, and I can control the UPS settings (ie: turn on/off audible alarm when on battery power). When I get a chance, I will configure it to shut down after five minutes on battery, and see if my server shuts down gracefully.
That brings up another question... Is it possible to have my server (a Dell Poweredge T110) power itself on when commercial power is restored ? There is a BIOS setting that causes the machine to resume the same state (powered on or off) when power is restored, but the server will not have shut down because power failed. It will have shut down because the PowerChute software told it to shut down. In fact, in a scenario such as a ten minute power failure, where Powerchute shuts down the server five minutes into the event, the line voltage at the UPS battery-supplied receptacles will have never failed. Could someone clarify this issue for me ? I would think it's impossible for the UPS to issue a power-on command to a computer that is powered off. Does a little robot crawl out of the UPS, walk over to my server, and press the ON/OFF button ?
: -- )
Message was edited by: SineWave
Posted: 2021-06-29 05:20 AM
This reply was originally posted by Angela on APC forums on 1/27/2011
User | Count |
---|---|
2125 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.