Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84719members
354116posts

Burning out UPS power

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
NetServices_apc
Cadet
0 Likes
2
186

Burning out UPS power

This was originally posted on APC forums on 2/3/2009


I am in a manufacturing environment. My servers are powered by several APC UPS's. Regardless of the model they last between 3 and 6 months. After which time I need to replace the batteries or the entire UPS. I've gone through 5 or 6 already.

I am confident this is a utility power condition that is causing the problem but I need a way to prove it. Are there any tools that are available to show I have poor quality or insufficient utility power? In past empoloyment just using the Power Chute reports I was able to make my case. But now I need more.

Are there any suggestions? Thank you in advance.

Tags (4)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
186

Re: Burning out UPS power

This reply was originally posted by Tim on APC forums on 2/4/2009


Also, something to try perhaps...

Most power companies will at your request put a power monitor on the circuit if you believe it is providing poor/disruptive power. If they wont, or it could be an internal issue due to the manufacturing equipment dumping allot of distortion on the lines or causing constant brownout conditions, you can always look into getting one yourself or as I Picked said, something like an O-Scope.

Otherwise we can look into the type of unit you have as mentioned, but you may find that to sufficiently point a finger at any particular issue, a good passive circuit monitor may be your best bet.

You could do a google search for a power circuit quality monitor, that should get you started if you choose to go that route.

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
186

Re: Burning out UPS power

This reply was originally posted by Angela on APC forums on 2/3/2009


what types of UPSs are you using? are these Back UPS, Smart UPS, etc

i know a lot of people/electricians use oscilloscopes in this situation to see if there is strange voltage, sine wave impurities, etc

but what exactly is happening to these when they fail? are they not turning on anymore, not going to battery during an outage, etc? any more information will help us see if we have any ideas.

thanks!

BillP
Administrator Administrator
Administrator
0 Likes
0
187

Re: Burning out UPS power

This reply was originally posted by Tim on APC forums on 2/4/2009


Also, something to try perhaps...

Most power companies will at your request put a power monitor on the circuit if you believe it is providing poor/disruptive power. If they wont, or it could be an internal issue due to the manufacturing equipment dumping allot of distortion on the lines or causing constant brownout conditions, you can always look into getting one yourself or as I Picked said, something like an O-Scope.

Otherwise we can look into the type of unit you have as mentioned, but you may find that to sufficiently point a finger at any particular issue, a good passive circuit monitor may be your best bet.

You could do a google search for a power circuit quality monitor, that should get you started if you choose to go that route.