Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84598members
353865posts

Boot PC after Power Down

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
mullfreak_apc
Crewman
Crewman
0 Likes
2
71

Boot PC after Power Down

This was originally posted on APC forums on 4/25/2009


Hi there,

i use a APC Back-UPS ES 700 with a ASUS Pundit P4 Barebone on the Battery Backup-Side.

When i shutdown Power the APC runs perfectly and shutdown the Windows XP on the ASUS Barebone. But when i Power On the ASUS dont boot up. If i dont use the APC the boot up works perfect when i power up the ASUS Barebone.

Why is the Power-Up-Function of the Barebone not working on the APC?

Greetings
Markus


Accepted Solutions
mullfreak_apc
Crewman
Crewman
0 Likes
0
71

Re: Boot PC after Power Down

This was originally posted on APC forums on 4/27/2009


Hi Erasmus,

thank you for your reply. Today i have solved the problem.
The APC must be complete empty. Then when power switch back to the APC the ASUS Barebone boots perfect.


Mull

See Answer In Context

2 Replies 2
Erasmus_apc
Sisko
Sisko
0 Likes
0
71

Re: Boot PC after Power Down

This was originally posted on APC forums on 4/27/2009


I would just like to clarify your test timeline, correct me if I am wrong:

Asus Barebone is turned ON, APC ES 700 is also ON and plugged into the wall.
APC ES 700 is unplugged from the wall.
APC ES 700 and software shut down Windows XP and Asus PC is turned off.
?? APC ES 700 turns itself off due to low batt ??
?? You plug the ES 700 back in and turn it on ??
?? Try to turn Asus Barebone back on and it does not turn on ??

Additionally, are you just hitting the power button on the Asus PC, or are you trying to remote start somehow? Are you trying to start the Asus PC automatically by using the APC ES 700 as a "power switch"?

mullfreak_apc
Crewman
Crewman
0 Likes
0
72

Re: Boot PC after Power Down

This was originally posted on APC forums on 4/27/2009


Hi Erasmus,

thank you for your reply. Today i have solved the problem.
The APC must be complete empty. Then when power switch back to the APC the ASUS Barebone boots perfect.


Mull