Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84839members
354298posts

Back-Ups XS1300LCD: Battery Fully Charged-Meter Shows 1 Bar Down?

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
jcuervo_apc
Crewman
Crewman
0 Likes
1
131

Back-Ups XS1300LCD: Battery Fully Charged-Meter Shows 1 Bar Down?

This was originally posted on APC forums on 9/7/2011


I recently had to change the batteries in my Back-UPS XS1300LCD, which like most UPS batteries, seemed to go bad shortly after the warranty ran out. Everything seems to work as normal except that when the batteries should be fully charged, the battery meter on the lcd display shows 1 bar down. It only seems to happen if you let it charge with the UPS turned on. If you turn it off from the button on the front and let it sit and charge for a while, the battery meter will then stay at full bars when turned back on.
I ran the batteries all the way down under load (a tv and a lamp) and then let them recharge, with the UPS turned on, and I got the same results with the meter bar. The run times seem to be about the same as with the old batteries, it shows about 140 minutes with a 30w load and didn't falter or die off quickly when I turned on the computer which brought the run times down to around 60 minutes. So from what I can tell, the UPS runs fine on battery power, my only concern is that because the battery meter never shows full (unless switched off for a while), that the unit could be trying to overcharge the batteries. The UPS does seem a bit warm, but I'm not sure if it's any warmer then it was before I swapped the batteries. It's not scorching hot or anything, but pretty warm to the touch.
Is this a problem or is it nothing I should be worried about? Does the battery meter not being full even indicate if it's still charging? Would there be any benefits to installing Powerchute to diagnose this problem?

Thank you for any answers.

Message was edited by: jcuervo

Message was edited by: jcuervo


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
131

Re: Back-Ups XS1300LCD: Battery Fully Charged-Meter Shows 1 Bar Down?

This reply was originally posted by Bernard on APC forums on 9/7/2011


Hi jcuervo,

Are you using a genuine APC battery? I suggest that you brain dead the UPS. Instructions here then check if the battery meter stays the same or not. You can also install Powerchute Personal Edition so you can see the percentage of the battery charge via the GUI.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
132

Re: Back-Ups XS1300LCD: Battery Fully Charged-Meter Shows 1 Bar Down?

This reply was originally posted by Bernard on APC forums on 9/7/2011


Hi jcuervo,

Are you using a genuine APC battery? I suggest that you brain dead the UPS. Instructions here then check if the battery meter stays the same or not. You can also install Powerchute Personal Edition so you can see the percentage of the battery charge via the GUI.