Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
It's your place to connect with experts and peers, get continuous support, and share knowledge.
Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-28 06:38 PM
This was originally posted on APC forums on 11/19/2020
Hi!
I have a Back-UPS Pro 550. After replacing the battery, I realised that my unit was not charging the battery anymore when powered ON. Tests I have conducted so far:
Based on the above it seems to indicate that charging circuit is OK, but it might be a SW issue or some failing sensor that cuts battery charging ? Is there any reset function or FW update that I could apply ? Anything else I could check / do to fix it ?
The unit is around 5 years old so not covered by warranty but still not that old 🙂
Thanks
Posted: 2021-06-28 06:39 PM
This was originally posted on APC forums on 1/6/2021
On 11/19/2020 12:19 PM, Bill said:You can try and brain dead the UPS to reset it.
Hi, thanks for the replies. I did try a brain dead reset + another type of reset I find on the internet, no success.
After opening the device I located a bad capacitor (see picture).
After replacing it, the charging process of the Battery is working again!
Thanks for the quick answers and the help.
Posted: 2021-06-28 06:38 PM
This reply was originally posted by Bill on APC forums on 11/19/2020
Hi,
You can try and brain dead the UPS to reset it.
See Schneider Electric FAQ FA158947 for instruction.
Posted: 2021-06-28 06:38 PM
This reply was originally posted by Scott on APC forums on 11/20/2020
the basic troubleshooting steps for the APC Back-UPS Pro with ... The Back-UPS is not connected to AC power, there is no AC power ... The battery will not charge if the temperature is over 50 degrees Celsius
Posted: 2021-06-28 06:39 PM
This was originally posted on APC forums on 1/6/2021
On 11/19/2020 12:19 PM, Bill said:You can try and brain dead the UPS to reset it.
Hi, thanks for the replies. I did try a brain dead reset + another type of reset I find on the internet, no success.
After opening the device I located a bad capacitor (see picture).
After replacing it, the charging process of the Battery is working again!
Thanks for the quick answers and the help.
Posted: 2021-06-28 06:39 PM
This was originally posted on APC forums on 1/13/2021
I have the same problem with this model.
APC wont do anything. It seems to be a problem with this model.
I will give a try to search for the capacitor. Thx for the input.
Posted: 2022-01-27 07:37 AM
Hi. I have the same problem with the same model. Which capacitor have you replaced?
Posted: 2022-01-30 10:05 AM
Hi,
I´m also facing the same problem. After opening the device I found the same capacitor being dead as in the picture. You can recognize a dead capacitor by its curved top. In my device its labeled as the capacitor C18. You´ll need a 330uF 35V ELKO for that.
Posted: 2022-02-11 07:25 AM
Hi ,
it also help me , but change two capacitors not only one
Posted: 2022-02-28 03:54 AM . Last Modified: 2022-02-28 04:22 AM
I have a similar problem:
Battery charging only during OFF and when ON battery is draining slowly even through connected to AC Mains input.
Got it open and capacitors seem fine
Any other suggestion?
Posted: 2022-02-28 11:56 AM
Hi ,
one capacitor in my ups looking fine but is only 270 uF and not working properly. After that i change it with new one 330 uF ups is working fine , only one capacitor is looking damaged but i changed two of us.
User | Count |
---|---|
2124 | |
88 | |
83 | |
83 | |
82 | |
79 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.