Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84702members
354078posts

BR1500GI / Back-UPS Pro very hot

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
sunnyville_apc
Crewman
Crewman
0 Likes
2
166

BR1500GI / Back-UPS Pro very hot

This was originally posted on APC forums on 4/12/2011


Hi!

I received my Back Ups Pro 1500 today, brand new. I had previously read a lot about the incredibly loud fans that stay on for hours, etc etc etc.
Well, I am hereby asking the community wether my unit could be defective:
The fan has not come on at all yet while charging. When I unplug the unit from the wall, thereby simulating a power failure, the fan comes on, but no sooner do I plug the device back in, the fan switches off.
My concern is the amount of heat I can feel coming out of the grills on the top of the unit - should the fan not kick in? I heard something somewhere about the fan supposedly running during charging, and once on, for a minimum length of 3 hours. Is this no longer the case? Could my unit overheat, or has it got protection against overheating?

thank you in advance for your replies - this is my first UPS so still lacking knowledge 😉

Message was edited by: sunnyville


Accepted Solutions
sunnyville_apc
Crewman
Crewman
0 Likes
0
166

Re: BR1500GI / Back-UPS Pro very hot

This was originally posted on APC forums on 4/14/2011


thanks, it does help! I am now at ease 😉

See Answer In Context

2 Replies 2
R2_apc
Commander
Commander
0 Likes
0
166

Re: BR1500GI / Back-UPS Pro very hot

This was originally posted on APC forums on 4/14/2011


Hi sunnyville, for these back ups pro units the fan will turn on for one of two reasons. The first is if unit is running on battery, and the second is if the unit is using its AVR functionality (boosting or trimming voltage). If the unit is not performing one of these functions, then that fan should not be running. It is possible that if a unit is placed in an environment with fluctuating voltage (i.e. the voltage swings high or low causing the AVR to kick in), that the fan would run for long periods time depending upon how long the voltage is "out of tolerance". This can usually be alleviated by changing the sensitivity of the unit to allow for a wider range of acceptable voltage (thereby stopping the unit from using its AVR function). Hope this helps.

sunnyville_apc
Crewman
Crewman
0 Likes
0
167

Re: BR1500GI / Back-UPS Pro very hot

This was originally posted on APC forums on 4/14/2011


thanks, it does help! I am now at ease 😉