Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84483members
353699posts

BR1000G or BR1500G for me?

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
74

BR1000G or BR1500G for me?

This question was originally posted by insoc on APC forums on 7/22/2013


Hello. I am planning to connect to the UPS a 32" LED HDTV (posible upgrade to a 40") and a PS3 and upgrade to the PS4 when it comes out. Additionaly I will connect some self powered 2.1 or 5.1 speakers. AVR and other TRIM features are a must. For those needs will the BR1000G suffice or would I better with a BR1500? Is there something apart from watts capacity tan the BR1500G provides over the BR1000G? Which would you choose? Thank you!!!


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
74

Re: BR1000G or BR1500G for me?

This reply was originally posted by Secret on APC forums on 7/23/2013


Beyond watt capacity, the BR1500G has a slightly larger battery which would provide greater runtime during power issues. I personally would recommend the BR1500G, as it will allow enough room for future expansion.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
75

Re: BR1000G or BR1500G for me?

This reply was originally posted by Secret on APC forums on 7/23/2013


Beyond watt capacity, the BR1500G has a slightly larger battery which would provide greater runtime during power issues. I personally would recommend the BR1500G, as it will allow enough room for future expansion.