Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84318members
353478posts

BN650M1-CA vs. BE600M1

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
fasterisbest_apc
Cadet
0 Likes
1
279

BN650M1-CA vs. BE600M1

This was originally posted on APC forums on 11/29/2019


Can anyone (from APC) tell me why I should buy one of these over the other?

As far as I can tell they are both almost identical. However the BE model has something called SVHCs (whatever that is) and the BN model does not. 

Thanks.

Attachments
Tags (2)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
279

Re: BN650M1-CA vs. BE600M1

This reply was originally posted by Thomas on APC forums on 12/2/2019


Hi Jamie,

There is very little difference between the two models. The biggest difference would be that the UPS capacity on the BN650M1 is 50VA more than the BE600M1. I have added the specifications for both models below.

0vyDhjdgRDwtOv1NBlLuUg%3D%3D.png

Regards,

Tom

See Answer In Context

Attachments
1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
280

Re: BN650M1-CA vs. BE600M1

This reply was originally posted by Thomas on APC forums on 12/2/2019


Hi Jamie,

There is very little difference between the two models. The biggest difference would be that the UPS capacity on the BN650M1 is 50VA more than the BE600M1. I have added the specifications for both models below.

0vyDhjdgRDwtOv1NBlLuUg%3D%3D.png

Regards,

Tom

Attachments