Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84255members
353353posts

BE750G Problem

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
momix803_apc
Cadet
0 Likes
1
110

BE750G Problem

This was originally posted on APC forums on 6/19/2013


I just got four BE750G's... on one of them the 'Master Enable' light is on... But, the power light is NOT on... all of the others, both lights are lit... all four are working... just the one, is working, but has no power light...

It's strange... What could be wrong with it???

The only difference that I'm aware of is that all are connected to Windows 8 computers... and the strangely acting one is connected to Kubuntu 13.04 - 64bit computer...

So, what could the problem be, and is there a way to fix it???


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
110

Re: BE750G Problem

This reply was originally posted by Angela on APC forums on 6/19/2013


I just want to double check - did you see that LED ever work? There is no reason that they should be different and the only thing coming to mind is a bad LED. It seems very improbable but I suppose it could happen. It certainly does not matter what OS or what you have connected to it (and if you felt otherwise, you could try swapping them between your systems, if possible) but I'd have to lean towards that bad LED.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
111

Re: BE750G Problem

This reply was originally posted by Angela on APC forums on 6/19/2013


I just want to double check - did you see that LED ever work? There is no reason that they should be different and the only thing coming to mind is a bad LED. It seems very improbable but I suppose it could happen. It certainly does not matter what OS or what you have connected to it (and if you felt otherwise, you could try swapping them between your systems, if possible) but I'd have to lean towards that bad LED.