Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354354posts

Another Question - General, this time

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
JDG213_apc
Cadet
0 Likes
1
36

Another Question - General, this time

This was originally posted on APC forums on 8/11/2012


What does the number (e.g., the "600" in an APC 600) signify?

Disregarding the power capabilities of the battery backup, is there a wattage maximum for surge protection?

Disregarding both battery backup & surge protection, is there a wattage maximum for simple power usage (e.g., number of watts the unit will safely pull to power several different peripherals)?

Thanks


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
36

Re: Another Question - General, this time

This reply was originally posted by Chris on APC forums on 8/14/2012


600 would be the VA(volt amps) capacity. You may want to look at the below link if you have questions on the VA rating versus the watt rating.

http://nam-en.apc.com/app/answers/detail/a_id/1503/kw/volt%20amps

As far as this would question, it may depend on the model #, Do you have a model # from the white sticker on the unit?


The capacity of the unit determines how much power can be used. Even if the circuit the back up is plugged into is rated for 15a, the UPS itself limits the amount or power it will output.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
37

Re: Another Question - General, this time

This reply was originally posted by Chris on APC forums on 8/14/2012


600 would be the VA(volt amps) capacity. You may want to look at the below link if you have questions on the VA rating versus the watt rating.

http://nam-en.apc.com/app/answers/detail/a_id/1503/kw/volt%20amps

As far as this would question, it may depend on the model #, Do you have a model # from the white sticker on the unit?


The capacity of the unit determines how much power can be used. Even if the circuit the back up is plugged into is rated for 15a, the UPS itself limits the amount or power it will output.