Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354354posts

Allowable fan clearance for Back-UPS 1500

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
ByteCrawler_apc
Cadet
0 Likes
1
226

Allowable fan clearance for Back-UPS 1500

This was originally posted on APC forums on 7/12/2015


I have a Back-UPS 1500 under my desk and that area is starting to get a little crowded. There are fans on both sides and the top of the unit which makes me very hesitant to put it up against a wall or the side of the desk. How much clearance do I need on the sides and top of the unit to ensure adequate cooling?

Also, I'm thinking of adding an additional battery pack. In the documentation, this pack is shown as being placed flush along side the main unit. Does this change the clearance required for the other fans?


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
226

Re: Allowable fan clearance for Back-UPS 1500

This reply was originally posted by Angela on APC forums on 7/13/2015


I have mine under my desk and I do just fine with about 3-4 inches clearance on each side. I would say whatever is needed to keep the ambient temp of the unit closest to 70-75ºF as possible. Beyond my own anecdotal information and general experience working with UPSs, I don't know of any "official" information regarding fan clearance.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
227

Re: Allowable fan clearance for Back-UPS 1500

This reply was originally posted by Angela on APC forums on 7/13/2015


I have mine under my desk and I do just fine with about 3-4 inches clearance on each side. I would say whatever is needed to keep the ambient temp of the unit closest to 70-75ºF as possible. Beyond my own anecdotal information and general experience working with UPSs, I don't know of any "official" information regarding fan clearance.