Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84722members
354123posts

Advice for UPS for laptop

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

inachot_apc
Cadet
0 Likes
0
70

Advice for UPS for laptop

This was originally posted on APC forums on 5/30/2012


Hello all!
I need a UPS for a gaming laptop and I really don't know much about UPS or wattage or VA, but I know that I need a very reliable UPS. The specifications of the AC adapter of the laptop are Output: 19.5 V DC, 7.7 A, 150W, Input:100~240 V AC, 50/60 Hz universal.
In a couple of months I will be in Argentina, and I know for a fact that the power there is alternating current 220, and it is super unstable, low voltages are extremely common,spikes and surges are crazy. I once had all my electronic appliances wasted because I was getting 330 instead of 220 (that's what my father said using a tester). I am not really interested in prolonging the use of the laptop when there is a power outage, I want to protect the laptop from spikes, low voltages and surges. So my question is what kind of VA capacity should I look for in the UPS? Is there a UPS that comes to mind that fits my needs?
Thank you a lot!!
InachoT

Tags (3)