Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

APC BE350 G constant alarm LED blinking red

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • APC BE350 G constant alarm LED blinking red
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2150
Teken
Teken
144
Techie_apc
Techie_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
dandy47
dandy47
Explorer

Posted: ‎2026-06-16 09:57 AM

0 Likes
4
245
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
Posted: ‎2026-06-16 09:57 AM

APC BE350 G constant alarm LED blinking red

Getting a constant squeal alarm and red LED blinking. When I check the unplugged battery it shows 13,55v. When I connect the battery, it shows same voltage. Turn the unit on while unplugged from 115v it still shows voltage fluctuating between 13.45 and 13.55 . When I plug the APC to 115v it still shows same voltage fluctuating. No load connected with all tests.
 
I left it off but plugged in with no load attached for a day.  Then turned it on. The green LED was blinking and the squeal waited maybe 5 seconds before sounding and the blinking LED turned red.
 
So, is it the battery or a bad unit?

Labels
  • Labels:
  • Back-UPS & Surge Protectors
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 4
Teken
Teken
Champion

Posted: ‎2026-06-17 08:02 AM

0 Likes
3
243
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
Posted: ‎2026-06-17 08:02 AM

Download, install, and connect the unit to a computer system running APC PCSS:

 

The Power Chute Software Program is at the very bottom of the page.

 

https://www.se.com/ca/en/product/BE350G/apc-backups-es-350va-120v/

 

Once the two systems are connected and PCSS software is running. Allow it to run for a minimum of 24 hours or when the application indicates what the error code / fault is.

 

Please review this APC FAQ to download the logs from the application and upload the same to the forum for review:

 

https://www.se.com/us/en/faqs/FA159672/

 

How old is the unit and RBC (Battery) in the system? Provide the serial number of the unit and a picture of the internal RBC out of the unit.

 

Clearly showing the production date of the battery and vendor sticker.

 

Questions Ask . . . 👍

Reply

Link copied. Please paste this link to share this article on your social media post.

dandy47
dandy47
Explorer

Posted: ‎2026-06-19 08:56 AM

In response to Teken
0 Likes
2
202
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
Posted: ‎2026-06-19 08:56 AM

Tried to install the PowerChute software but it does not see a connected UPS. Cannot connect the UPS because the 940-0127B cable (number on the USB end) I have will not connect to the port on the UPS. Think the UPS was purchased in 2019 and it is the original battery, I think. I included the cable in the battery pic. I see no date on the battery.

Attachments
Reply

Link copied. Please paste this link to share this article on your social media post.

Teken
Teken
Champion

Posted: ‎2026-06-22 04:48 AM . Last Modified: ‎2026-06-22 04:48 AM

In response to dandy47
0 Likes
1
200
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
Posted: ‎2026-06-22 04:48 AM . Last Modified: ‎2026-06-22 04:48 AM

Can you provide a photo of the available ports on the unit. As the user manual only indicates two RJ11 / 12 for telephone surge protection and no Data port for APC Power Chute Software.

 

As it relates to the RBC can you provide a photo for the remaining sides for review. The production date is normally on the narrow side opposite of the battery terminals.

 

It will normally be a multi colour yellow sticker which has a alphanumeric numbers.

 

NOTE: The RBC is rated to provide 2-5 years of service life based on usage, temperature, and environmental conditions. The internal raw cells are designed to provide 260 cycles subject to the same caveats as above.

 

Your RBC is seven years old and is more than likely EOL and needs to be replaced.

 

Questions Ask . . . 👍

Reply

Link copied. Please paste this link to share this article on your social media post.

dandy47
dandy47
Explorer

Posted: ‎2026-06-23 04:38 AM

In response to Teken
0 Likes
0
181
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
Posted: ‎2026-06-23 04:38 AM

I was wondering same thing about the ports.

 

Only one side of RBC has anything on it. It's a stamped number (MF27GB) in the plastic case as seen in the picture. There is no yellow sticker.

 

I figured the battery is EOL but since it was measuring full voltage it had me wondering. Wasn't wanting to buy new battery for a faulty unit I could help it.

 

Only thing plugged in on this unit is a modem and router.

 

We did have a few hour power outage a few weeks prior to this unit acting up. But it did come back up after power was restored. No other problems in the house from the power outage so don't think there was any surge. 

 

Thanks for your help.

 

 

Attachments
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.