Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84599members
353867posts

4 Port USB hub model 19500SG-1G

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
bakes99_apc
Crewman
Crewman
0 Likes
1
180

4 Port USB hub model 19500SG-1G

This was originally posted on APC forums on 3/30/2010


Just purchased this USB hub and did not come with any instructions. The online instructions state the same model #, but appears to be quite different looking hub than the one I received.

This one comes with a power adapter. In the instructions it states that an orange light appears when the hub is receiving power from the power source at the correct level. Mine does not light up orange at any time. Just a red light when power is reaching the unit. The red light will illuminate whether the AC adapter is plugged in or not, as long as the USB adapter is plugged into my macbook. I can unplug the ac adapter and the red light will remain on. I assume that its drawing all its power from my Macbook at this point.

My questions are, is there any way to tell if the unit is drawing all its power from the adapter or if its drawing any from my Macbook.

Getting a new Imac. When I put my Imac to sleep, do I have to disconnect the USB hub or can I leave it plugged in. If I leave it plugged in, will it still draw power from my Imac especially when the Imac wakes up or will it totally rely on the included adapter.
That's about it
Thanks in advance

Attachments

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
180

Re: 4 Port USB hub model 19500SG-1G

This reply was originally posted by Laurie on APC forums on 4/6/2010


Yes, the hub can draw power from your computer. It has the adapter because, depending on what you plug into the hub, it may not be able to draw enough power from a single USB port on your computer. For example, 4 USB mice will work fine but I doubt 4 USB scanners would.

There isn't really any way to tell where it's drawing its power from since it's more a matter of what you're plugging into the hub. If you have it plugged into your computer only and it's powering everything on the hub fine, then it's drawing all of the power from the computer. If the devices in the hub aren't powering on, then you need to use the adapter to support those devices.

I'm not sure about the power settings on the iMac in terms of sleep mode. I know my PC will pass power through the USB ports in sleep mode, even when it's turned off - enough to charge a cell phone anyway - but no idea what Mac does for power settings. I don't see why you would need to disconnect it from your computer either way. Depending on what you're most concerned about, I would probably just leave the hub's adapter plugged in, assuming you're connecting enough devices to require it.

Hope that helps. 🙂

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
181

Re: 4 Port USB hub model 19500SG-1G

This reply was originally posted by Laurie on APC forums on 4/6/2010


Yes, the hub can draw power from your computer. It has the adapter because, depending on what you plug into the hub, it may not be able to draw enough power from a single USB port on your computer. For example, 4 USB mice will work fine but I doubt 4 USB scanners would.

There isn't really any way to tell where it's drawing its power from since it's more a matter of what you're plugging into the hub. If you have it plugged into your computer only and it's powering everything on the hub fine, then it's drawing all of the power from the computer. If the devices in the hub aren't powering on, then you need to use the adapter to support those devices.

I'm not sure about the power settings on the iMac in terms of sleep mode. I know my PC will pass power through the USB ports in sleep mode, even when it's turned off - enough to charge a cell phone anyway - but no idea what Mac does for power settings. I don't see why you would need to disconnect it from your computer either way. Depending on what you're most concerned about, I would probably just leave the hub's adapter plugged in, assuming you're connecting enough devices to require it.

Hope that helps. 🙂