Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84826members
354280posts

350 - Just want to use it as a surge protector with no battery...

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
Integraoligist_apc
Crewman
Crewman
0 Likes
4
235

350 - Just want to use it as a surge protector with no battery...

This was originally posted on APC forums on 11/25/2014


So I've got 4 of the UPS 350s which have all beeped annoyingly because the batteries are shot in them as they are all 6 years old. BUT I do not need battery backup... I just want to use them as a standard Surge Protector.

I removed the batteries completely and assumed they would see that it's not connected so it shouldnt beep... nope, after 5 days of them all being plugged in and running things, one decides to beeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeeep. So I have to pull it from the wall for a few seconds and plug it back in to stop.

Is there any possible way to use these things without that beeping? Even when they were new they would still act stupid with the beeping.

Do I need to open them all and rip out the speaker on them to fix this or what?

Thanks!


Accepted Solutions
Integraoligist_apc
Crewman
Crewman
0 Likes
0
236

Re: 350 - Just want to use it as a surge protector with no battery...

This was originally posted on APC forums on 12/3/2014


Thanks for that info. As when we bought all of these the batteries did not last more then just a few months before the "self test" started to go array on all of them... the the fact that the batteries are closer to what a new unit will cost, we're just not going to go the APC route and probably just buy terminator protectors as we did at our other shops and never had an issue.

Thanks for the help.

See Answer In Context

4 Replies 4
BillP
Administrator Administrator
Administrator
0 Likes
0
236

Re: 350 - Just want to use it as a surge protector with no battery...

This reply was originally posted by Angela on APC forums on 12/1/2014


Hi,


Can you clarify the exact model from the back or bottom of them? It'd show it on a white sticker - something like BE350G or similar. Some units have the capability to disable the beeping for certain situations but I'd have to check once I know the specific model since we have a few generations of 350VA models.

Integraoligist_apc
Crewman
Crewman
0 Likes
0
236

Re: 350 - Just want to use it as a surge protector with no battery...

This was originally posted on APC forums on 12/2/2014


BE350R

Thanks!

BillP
Administrator Administrator
Administrator
0 Likes
0
236

Re: 350 - Just want to use it as a surge protector with no battery...

This reply was originally posted by Secret on APC forums on 12/2/2014


Hi Integraolgist, The unit is cerainly still capable of providing you limited surge suppression without the internal battery installed, however it is not recommended you use the unit in this fashion. The beeping your hearing, is likely resulting from a failed Automatic selftest which occurs every 14days. When it attempts to run the selftest and see's that there is no internal battery, the unit enters a fault conditon emitting a constant tone. The tone is emitted from a small solid state component which is physically soldered to the internal PCB board. I would not recommend altering this circuitry and would rather suggest you replace the internal batteries or procure a suitable surge arresting device.

http://www.apc.com/products/family/index.cfm?id=220

Regards,

Secretsquirrel

Integraoligist_apc
Crewman
Crewman
0 Likes
0
237

Re: 350 - Just want to use it as a surge protector with no battery...

This was originally posted on APC forums on 12/3/2014


Thanks for that info. As when we bought all of these the batteries did not last more then just a few months before the "self test" started to go array on all of them... the the fact that the batteries are closer to what a new unit will cost, we're just not going to go the APC route and probably just buy terminator protectors as we did at our other shops and never had an issue.

Thanks for the help.