APC UPS Data Center & Enterprise Solutions Forum
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Posted: 2021-07-01 02:00 AM
This was originally posted on APC forums on 1/10/2013
All,
I have written a template for the UPS devices throughout the organizations network and i was just wondering if i was to upload the template to the UPS during working hours that it wouldn't hang, interrupt or cause any problems/issues.
So really I'm asking if I upload a template will it cause any issues?
Thanks,
Thomas.
Posted: 2021-07-01 02:00 AM
This reply was originally posted by Angela on APC forums on 1/11/2013
yes, if you are modifying IP, subnet, Gateway, or bootmode (or just one of them), you will need the override=MAC address for the particular card. for anything you don't want to modify, you can just remove the keyword (item before 😃 and value (item after 😃 completely and the card won't do anything with it. it can also save space in the file and save time too for the card to process.
Posted: 2021-07-01 02:00 AM
This was originally posted on APC forums on 1/14/2013
Thank you very much - I carried out the work on Sunday and as described it worked without hitch in the most part.
Thanks again for your support in this matter.
Posted: 2021-07-01 02:00 AM
This reply was originally posted by Chris on APC forums on 1/10/2013
I assume you're referring to a config(config.ini) file? If so, the worst thing that would ever happen would be a warm start due to high network traffic. A warm start only reboots the card and not the UPS(outlet, usually due to network traffic This is a worst case scenario though. I wouldn't expect a config.ini upload to cause even a warmstart.
Posted: 2021-07-01 02:00 AM
This reply was originally posted by Angela on APC forums on 1/10/2013
depending on any changes that need to be made, just be aware it could take 3-5 minutes to apply to each card too but hopefully not that long.
Posted: 2021-07-01 02:00 AM
This was originally posted on APC forums on 1/10/2013
Thanks for the replies guys - I'll give this a bash in the next few days and will come back to you just to let you know how I get on.
Cheers
Posted: 2021-07-01 02:00 AM
This was originally posted on APC forums on 1/11/2013
The below is part of my template - I'm hoping it's right. I'm going to be configuring around 30/40 of the UPS devices on Sunday and plan to create individual .ini files with just the hostname/IP add changed but wasnt sure if I needed the Override part of the config...
Thanks again for all your help it really is appreciated
Override=00 C0 B7 D0 F5 24
SystemIP=172.16.2.207
SubnetMask=255.255.255.0
DefaultGateway=172.16.2.1
BootMode=Manual
HostName=gh5-r25-ups1
DomainName=
PortSpeed=Auto
DHCPBootpVendorClass=APC
DHCPBootpClientID=MAC
DHCPBootpUserClass=SUMX
BootpMaxRetries=4
BootpUserPriorSettings=enabled
DHCPMaxRetries=0
DHCPRequireCookie=enabled
BootModeTransition=enabled
Posted: 2021-07-01 02:00 AM
This was originally posted on APC forums on 1/11/2013
One last question guys - with my template do I need to have a specific mac address for each ini? i.e. the mac address of the device i am uploading to the device:
[NetworkTCP/IP]
Override=00 C0 B7 D2 XX XX ?
Sorry if that sounds daft.
Posted: 2021-07-01 02:00 AM
This reply was originally posted by Angela on APC forums on 1/11/2013
you don't need to have that unless you are applying certain settings such as IP, subnet, default gateway, and bootmode. it is a way to help prevent a user from mass configuring the same network settings to multiple cards. if the override=MAC ADDRESS does not equal the actual MAC of the card, it will not apply those settings i mentioned.
there are also certain UPS models where this applies and you'll see override=XX123456890 where that is the serial number of the UPS and if it doesnt match, it won't apply certain items like output voltage, transfer ranges, frequency, etc.
more info here-> http://www.apc.com/site/support/index.cfm/faq/ -> search for FA156136
Posted: 2021-07-01 02:00 AM
This reply was originally posted by Angela on APC forums on 1/11/2013
yes, if you are modifying IP, subnet, Gateway, or bootmode (or just one of them), you will need the override=MAC address for the particular card. for anything you don't want to modify, you can just remove the keyword (item before 😃 and value (item after 😃 completely and the card won't do anything with it. it can also save space in the file and save time too for the card to process.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.