Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84422members
353606posts

Rack PDU 7xxx command options

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
407

Rack PDU 7xxx command options

This question was originally posted by Dan on APC forums on 3/3/2020


We would like to create a web based set of events such as forcing a reboot on 7000 based ip pdu's. Rather than providing user logons and teaching users how to navigate what is a fairly easy menu we have been asked to create a central site to perform the tasks for users.

Our typ device is running rpdu v3.9.2 under AOS 3.9.2

Our 1st thought was to use a rest interface if one exists for the device as a worst case we thought of telnet and canned commands. ANy thoughts???

 

DAn

Tags (3)

Accepted Solutions
B-DoubleE_apc
Commander
Commander
0 Likes
0
407

Re: Rack PDU 7xxx command options

This was originally posted on APC forums on 3/3/2020


Hi Dan,

There are a few ways to interface with the PDU's that might help you. Switched rPDU's have a scripting interface that can be used to push commands, more info here: https://www.apc.com/us/en/faqs/FA156163/

rPDU's also support SNMP, so a web-based solution that would use SNMP OID's to set different values could also work.

See Answer In Context

1 Reply 1
B-DoubleE_apc
Commander
Commander
0 Likes
0
408

Re: Rack PDU 7xxx command options

This was originally posted on APC forums on 3/3/2020


Hi Dan,

There are a few ways to interface with the PDU's that might help you. Switched rPDU's have a scripting interface that can be used to push commands, more info here: https://www.apc.com/us/en/faqs/FA156163/

rPDU's also support SNMP, so a web-based solution that would use SNMP OID's to set different values could also work.