APC UPS Data Center & Enterprise Solutions Forum
Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.
Posted: 2021-06-30 11:17 PM
This was originally posted on APC forums on 2/8/2011
All,
I have purchased several BX1000G units. they are replacing old BK500 units.
id like to use the software for these new cats.
is it possible to individually plug in to each unit at anytime to get a reading from the units or must a computer stay attached to each one in order for the software to work properly?
i dont have the units set up to do any auto shut down of gear. i would just like to see if at any time i could just bring a laptop to any of the units, plug in the usb cable, and read the status of that unit..
make sense?
thank you in advance for any info. im using old school windows xp...
Posted: 2021-06-30 11:17 PM
This was originally posted on APC forums on 2/11/2011
ok so i am able to just plug up the laptop to these units and it will read them as one expects. this is good for me as i have these in different locations..
plus i had to upgrade 2 of these to the 1300 model so i could have more headroom on the load..
so thank you sir for your prompt response. hope the class was swell... 🙂
consider this issue handled...
Posted: 2021-06-30 11:17 PM
This reply was originally posted by Angela on APC forums on 2/11/2011
glad to hear.
Posted: 2021-06-30 11:17 PM
This was originally posted on APC forums on 2/9/2011
yes thank you. i do believe this information is helpful. i will follow your steps to the letter. thank you for posting. i i have any follow ups to this i will post and would hope you would be around to answer... i just received another unit today and im now going to launch these into service...
Posted: 2021-06-30 11:17 PM
This reply was originally posted by Angela on APC forums on 2/9/2011
yes, i believe that will work. when you install the PCPE software though, you need to have one of the UPS's connected so that the software will proceed with the installation. then, you can unplug it if you want but the PCPE software will tell you that it cannot communicate with the battery back up, which might be an annoying pop up you have to supress. but, each time you connect the UPS, it will read that particular UPS's information.
Posted: 2021-06-30 11:17 PM
This reply was originally posted by Angela on APC forums on 2/9/2011
yes, i will be around. i am providing training the next few days but i will try to come check the forum too.
Posted: 2021-06-30 11:17 PM
This was originally posted on APC forums on 2/11/2011
ok so i am able to just plug up the laptop to these units and it will read them as one expects. this is good for me as i have these in different locations..
plus i had to upgrade 2 of these to the 1300 model so i could have more headroom on the load..
so thank you sir for your prompt response. hope the class was swell... 🙂
consider this issue handled...
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.