New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
I am trying to configure two APC/Schneider NetShelter Rack PDU Advanced APDU10150ME units in Cascade mode so that both PDUs can be centrally monitored and managed through a single management IP address.
The objective is for PDU1 to operate as the Host, with PDU2 operating as the Guest and ultimately managed through PDU1 rather than requiring its own permanent management IP address.
Schneider documentation states that APDU10-series Rack PDUs support Cascade mode, allowing up to 32 Rack PDUs to be connected using one IP address, with information and data from Guest PDUs gathered by the Host PDU.
I understand this is different from Redundant Network Access (RNA), which is the default mode.
CURRENT CONFIGURATION
Originally both PDUs were operating in RNA mode.
Using the CLI, I found the following command:
dev cascade [rna/qna] [init] [create]
I changed both PDUs from RNA to QNA.
The Configuration Log confirms:
DaisyMode configuration is changed to QNA from RNA
Both PDUs now report:
SUCCESS Cascading unit number : 1 Cascading address list: 0 Cascade Mode : QNA
COMMANDS TESTED
On PDU1 I have run:
dev cascade qna create
The PDU responded:
SUCCESS Reboot required for change to take effect System Reboot now, Are you sure?(Y/N):Y
After the management controller rebooted, I checked:
dev cascade
and received:
SUCCESS Cascading unit number : 1 Cascading address list: 0 Cascade Mode : QNA
I have also run on PDU1:
dev cascade qna init
This was also successful and requested the management controller to reboot.
On PDU2 I have run:
dev cascade qna init
This was also accepted successfully and requested a reboot.
After all the changes and reboots, BOTH PDUs still individually report:
SUCCESS Cascading unit number : 1 Cascading address list: 0 Cascade Mode : QNA
Therefore neither unit appears to have become a Guest, and PDU1 does not display another member within its Cascading address list.
PHYSICAL CONNECTION TESTED
PDU1 currently has its normal management connection and address:
PDU1 Management IP: X.X.X.X
PDU2 currently has an independent management address for configuration and testing:
PDU2 Management IP: X.X.X.X
I have physically connected:
PDU1 ETH1 | | Standard Ethernet patch lead | PDU2 ETH1
Both units have been configured for QNA, but PDU2 is still not discovered or adopted by PDU1.
QUESTIONS
Could anyone familiar with APDU10/APDU10150ME cascading please confirm the exact supported procedure?
1. What is the correct physical cabling arrangement between two APDU10150ME PDUs?
For example:
PDU1 ETH1 -> PDU2 ETH1
or:
PDU1 ETH1 -> PDU2 ETH0
or is another physical arrangement required?
2. What exactly does QNA represent on the APDU10150ME?
The PDU Configuration Log specifically reports:
DaisyMode configuration is changed to QNA from RNA
3. What exactly do the following CLI commands do?
dev cascade qna init
dev cascade qna create
4. Which command should be executed on the Host PDU?
5. Which command should be executed on the Guest PDU?
6. What is the correct sequence for configuring the cascade?
or should the physical cascade connection already be present before running the CLI commands?
7. Does the Guest PDU initially require its own management IP/network connection while joining the cascade?
8. Once successfully joined, should the Guest PDU's independent management connection/IP be removed so that administration and monitoring occur entirely through the Host?
9. Both PDUs currently report:
Cascading unit number : 1
Should the Guest automatically receive a different Cascading unit number once successfully joined?
10. Both currently report:
Cascading address list: 0
What should the Cascading address list show for a successful two-PDU cascade?
11. Are there specific requirements for:
- Ethernet port selection - Cable type - Maximum cascade cable length - Firmware versions - Identical PDU SKUs - Host/Guest configuration order - Initial Guest addressing
12. Is there an additional Host/Guest adoption, discovery or pairing operation required after changing DaisyMode from RNA to QNA?
13. Is QNA the correct Cascade operating mode for these APDU10150ME units, or is there another configuration required in addition to QNA?
I am specifically looking for the procedure applicable to the APDU10/APDU10150ME generation.
I am aware that older APC AP8xxx Network Port Sharing uses a different IN/OUT port and terminator arrangement, so I do not want to apply the AP8xxx procedure to the APDU10150ME unless Schneider confirms it is applicable.
If anyone has a working APDU10150ME cascade, it would be extremely helpful if you could provide:
- Exact physical port-to-port cabling - Host CLI commands - Guest CLI commands - Exact init/create sequence - Required reboot order - Expected dev cascade output after successful joining - Screenshots of a working cascade - Any relevant Schneider documentation or configuration examples
Any assistance from someone who has successfully configured an APDU10/APDU10150ME Host/Guest cascade would be greatly appreciated.