This reply was originally posted by Angela on APC forums on 4/20/2011
hi,
here are some comments from APC, based on your post above:
The current version of PCBE (v9.01) available for download installs an obsolete and highly insecure version of Java -- JRE6u19 was superceded a full year ago and the current/secure version from Sun/Oracle is JRE6u24, with a total of five (5) JRE updates that are more recent than what's built into the PCBE installer. Furthermore, PCBE apparently requires that obsolete version it installs to function properly, and if it is manually removed (which must be done in Safe Mode to accomplish file deletions) PCBE won't function at all.
This is always the case when bundling a JRE in an application. When we update PCBE, we bundle the latest JRE at that time. PCBE 9.0.1 was a minor update to 9.0, so the JRE wasn't updated in this case. The JRE configuration tool on the website was created for this purpose. You can download the tool from this link:
http://www.apc.com/products/family/index.cfm?id=125Why isn't the downloadable installation file available on the APC website re-compiled on a timely basis to include the latest patched version of Java, say within a few days of a new Java release?
We would have to release a new version of PCBE every time a new JRE was released. If a JRE has significant vulnerabilities do we recommend customers to upgrade using the JRE upgrade tool and as stated above the JRE tool is available to anyone that does want to upgrade.
Why doesn't PCBE use an already-installed version of Java on a user's computer if it's more recent (and more secure) than what's embedded in the compiled installer, instead of forcing the obsolete version onto a user?
We have many customers want the JRE version to be fixed.
Why does APC think I should be willing to house an insecure Java version on any of my computers, given the potential security risks entailed by allowing that old version remain and become potentially available for use by some application other than PCBE (e.g., malware that managed to get by my layered-security screen)?
We are going in the direction of making the JRE either public or fixed and this will be implemented in a future release.