Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the new Schneider Electric Community! Community is now no longer part of Exchange, and is now rebranded under se.com. If you have any bookmarks and links saved, we request you to update them to ensure that you continue accessing our community from this new location. For any issues that you might encounter as part of this change, please reach out to SchneiderCommunity.Support@se.com, and the team will help to get your issues resolved.
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82414members
349923posts

Can I plug a bare RBC124 into a Back-UPS Pro 1500 as the external battery?

APC UPS Data Center Backup Solutions Forum

Schneider Electric support forum for Data Center UPS, software and services including our APC offers designed to share knowledge, installation, configuration, and general product use.

Solved
megnin_apc
Crewman
Crewman
0 Likes
2
173

Can I plug a bare RBC124 into a Back-UPS Pro 1500 as the external battery?

This was originally posted on APC forums on 12/23/2011


I just bought a Back-UPS Pro 1500 and an extra RBC124 battery pack thinking I would be able to plug that in to the external battery connector, a BR24BPG.

I already have the RBC124. Can I just plug it into the back of the Back-UPS Pro 1500? I have a connector that should work if the bare battery is okay to use instead of the BR24BPG unit. I got the connector off of a RBC32 battery pack and the plug fits the back of the 1500.

Tags (2)

Accepted Solutions
megnin_apc
Crewman
Crewman
0 Likes
0
173

Re: Can I plug a bare RBC124 into a Back-UPS Pro 1500 as the external battery?

This was originally posted on APC forums on 12/30/2011


Yes, please and thank you. I have the connector hooked up and it's ready to plug in.

If the BR24BPG external battery package is just four batteries in a box, then it seems like my two batteries without the box should work just fine. But, I don't know if the BR24BPG has any circuitry to assist in charging or anything like that.

Oh, from looking at the pictures in this blog, there's no circuitry whatsoever except for the fuse or resistor on the yellow wire. My connector also has a yellow wire, for whatever function it performs.
http://www.yourwarrantyisvoid.com/2009/10/27/breaking-into-apcs-br24bp-battery-pack/#comments

Message was edited by: megnin

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
173

Re: Can I plug a bare RBC124 into a Back-UPS Pro 1500 as the external battery?

This reply was originally posted by Chris on APC forums on 12/29/2011


This isn't something we can recommend however that doesn't mean it will not work. If anyone has any experience doing this, feel free to reply.

megnin_apc
Crewman
Crewman
0 Likes
0
174

Re: Can I plug a bare RBC124 into a Back-UPS Pro 1500 as the external battery?

This was originally posted on APC forums on 12/30/2011


Yes, please and thank you. I have the connector hooked up and it's ready to plug in.

If the BR24BPG external battery package is just four batteries in a box, then it seems like my two batteries without the box should work just fine. But, I don't know if the BR24BPG has any circuitry to assist in charging or anything like that.

Oh, from looking at the pictures in this blog, there's no circuitry whatsoever except for the fuse or resistor on the yellow wire. My connector also has a yellow wire, for whatever function it performs.
http://www.yourwarrantyisvoid.com/2009/10/27/breaking-into-apcs-br24bp-battery-pack/#comments

Message was edited by: megnin