Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the new Schneider Electric Community! Community is now no longer part of Exchange, and is now rebranded under se.com. If you have any bookmarks and links saved, we request you to update them to ensure that you continue accessing our community from this new location. For any issues that you might encounter as part of this change, please reach out to SchneiderCommunity.Support@se.com, and the team will help to get your issues resolved.
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82200members
349805posts

AR3100 front cable management

APC UPS Data Center Backup Solutions Forum

Schneider Electric support forum for Data Center UPS, software and services including our APC offers designed to share knowledge, installation, configuration, and general product use.

Solved
mrajdukovic_apc
Ensign
Ensign
0 Likes
1
99

AR3100 front cable management

This was originally posted on APC forums on 8/24/2016


Is it possible to put vertical cable manager in front of AR3100 or is it possible to move one vertical flange in front of the rack. I have a customer that owns an AR3100 and is in need of guiding cables from the front rather from the back.

Thanks for your help and advice

Tags (3)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
99

Re: AR3100 front cable management

This reply was originally posted by Ross on APC forums on 8/24/2016


Hello Nebojsa, 

Yes, in the NetShelter SX cabinets you can move the front and rear rails back and forth the entire length of the cabinet, and you can relocate the accessory mounting rails to the front if you prefer. You an even install them in the middle of the cabinet if you like! Or, if the customer needs to keep the existing accessory mounting rail in the rear we have two widths available as accessories. AR7502 is the standard (2 PDU wide) accessory rail. We also offer a narrow version (1 PDU wide) in AR7711. 

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
100

Re: AR3100 front cable management

This reply was originally posted by Ross on APC forums on 8/24/2016


Hello Nebojsa, 

Yes, in the NetShelter SX cabinets you can move the front and rear rails back and forth the entire length of the cabinet, and you can relocate the accessory mounting rails to the front if you prefer. You an even install them in the middle of the cabinet if you like! Or, if the customer needs to keep the existing accessory mounting rail in the rear we have two widths available as accessories. AR7502 is the standard (2 PDU wide) accessory rail. We also offer a narrow version (1 PDU wide) in AR7711.