Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the new Schneider Electric Community! Community is now no longer part of Exchange, and is now rebranded under se.com. If you have any bookmarks and links saved, we request you to update them to ensure that you continue accessing our community from this new location. For any issues that you might encounter as part of this change, please reach out to SchneiderCommunity.Support@se.com, and the team will help to get your issues resolved.
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82418members
349935posts

AP9630 looses IP lease from DHCP server

APC UPS Data Center Backup Solutions Forum

Schneider Electric support forum for Data Center UPS, software and services including our APC offers designed to share knowledge, installation, configuration, and general product use.

Solved
edmundsca_apc
Cadet
0 Likes
3
176

AP9630 looses IP lease from DHCP server

This was originally posted on APC forums on 10/15/2013


Hi,

I have a SMT1400 with a new AP9630 card with new 6.0.6 firmware.  I'm on a home network with a consumer grade Netgear router, and have an IP address reserved for the AP9630.  Setup and everything went fine with a few issues:

  1. The email notification only works with DHCP enabled, not manual TCP.
  2. SNMP notification only works with DHCP enable, not manual TCP.
  3. After 24 hours TCP/IP lease is up, the card looses network connection entirely and can only be reconnected by cold-starting the card.

Shouldn't I be able to manually set the IP address and the gateway, subnet (identical to how it's listed in the GUI).  This would be more stable, but it disables SNMP notification to my NAS and also eliminated email notification.

Thanks in advance for your help!


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
176

Re: AP9630 looses IP lease from DHCP server

This reply was originally posted by Angela on APC forums on 10/16/2013


Oh ok. Yes, that sounds right, you'd need to input your DNS manually.

Anyway, if you still wanted to attach log files, you can do so by starting a reply and clicking on "Use Advanced Editor" on the top right of the reply box which offers the attach file feature.

See Answer In Context

3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
0
176

Re: AP9630 looses IP lease from DHCP server

This reply was originally posted by Angela on APC forums on 10/15/2013


I am not sure what is causing this but no matter if you use DHCP, BOOTP, or Manual TCP/IP settings, this should all work. Most users do utilize manual settings versus DHCP and there are no widespread problems with this type of thing. So, there might be something else going on.

What NAS are you using? Does it require you to input the IP address of the NMC in?

If you'd like, I can take a look at your log files if you want to provide them. You can get a full dump of files from the web UI under About->Support and then select Generate Logs and after that is done, Download logs and then select "advanced editor" on your reply and attach the .tar file you receive.

edmundsca_apc
Cadet
0 Likes
0
176

Re: AP9630 looses IP lease from DHCP server

This was originally posted on APC forums on 10/16/2013


Hi Angela,

Thanks for your reply.  I'm happy to send you my log files, but don't see a button in this reply box to attach them.  I think I've solved my issue however in manually assigning the TCP/IP and assigning my router ip as the primary DNS.  This seems to be the thing I was missing.

Thanks much!

Chuck E.

BillP
Administrator Administrator
Administrator
0 Likes
0
177

Re: AP9630 looses IP lease from DHCP server

This reply was originally posted by Angela on APC forums on 10/16/2013


Oh ok. Yes, that sounds right, you'd need to input your DNS manually.

Anyway, if you still wanted to attach log files, you can do so by starting a reply and clicking on "Use Advanced Editor" on the top right of the reply box which offers the attach file feature.