Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84694members
354073posts

MC80_將HSC配置為DI和DO使用

臺灣施耐德工業自動化應用知識交流論壇

本論壇為交流施耐德電機工業自動化應用資訊,與業界夥伴互相分享、促進共同協作,發掘問題與解答。 This forum is addressing industrial automation design & engineering, operations, asset performance, cybersecurity and digital transformation for Plants & Machines.

James_Chang
Crewman Crewman
Crewman
0 Likes
0
249

MC80_將HSC配置為DI和DO使用

MC80 其模組中有HSC、DDM 和AI。 有時使用者需要更多的DI 和DO,
因此我們可以建議使用者將HSC 配置為DI 和DO 使用,HSC 0 可用做 6 x DI 與 2
xDO ,HSC 1 可用做 6 x DI 與 2 xDO.

Attachments
Tags (2)