The status LED’s (right hand side) will appear as follows: Off – The card is not receiving power or is in a boot up state. Solid Green – The card has valid IP settings Solid Orange – The card has a hardware failure. Flashing Green – The card does not have valid IP settings. Flashing Orange – The card is making BootP requests Alternating Green/Orange – (Rapidly) The card is booting up. (Slowly) The card is making a DHCP request. The Link/RX/TX LED’s (left hand side) will appear as follows: Off -The card is not receiving power -The card does not have a connected network cable -The device (switch/hub) connected to the Network Management Card is not active. Solid Green – The card is on a network that communicates at 10mbps. Solid Orange – The card is on a network that communicates at 100mbps. Flashing Green – The card is receiving data packets at 10mbps. Flashing Orange – The card is receiving data packets at 100mbps.